Part Number: AMP-PDK-EVM Dear TI Engineers,
I noticed that the user manual for this product contains the images of the board layouts but I could not locate the actual gerber files. Is it possible for TI to share the gerbers?
Thank you!
Part Number: AMP-PDK-EVM Other Parts Discussed in Thread: TLV6002 Tool/software: Hello,
Today, I came across a document by chance, and I found it to be very well written. However, there is a section where I believe the description might be incorrect…
Part Number: AMP-PDK-EVM Other Parts Discussed in Thread: OPA827 , ADS131M08 , OPA2140 Tool/software: Hi,
I am testing the AMP-PDK-EVM, with the SOIC-8 daughter board, I have a OPA827AID. When I test the voltage buffer, I am able to replicate the signal…
Hi Srinivasa,
What is your application? What does your signal chain look like? I think the calculations in this current sensing EVM user's guide may be useful to reference Section 4.1.3:
AMC-AMP-50A-EVM Evaluation board | TI.com
Best regards…
Part Number: AMP-PDK-EVM Tool/software: Hi
The request is actually for SKU AMP-PDK-SOT23-6 (but this part was coming up as "unrecognised in the Part Number field).
Could you please confirm SKU AMP-PDK-SOT23-6 i s CE ad if YES, please provide t he…
Part Number: SOT23-UNIV-AMP-EVM Other Parts Discussed in Thread: LMV321-N I am confused about the frequency for the PWM signal coming in. It is between 0 and 3.3 V. The C1 and R1 form a low pass filter. Which I calculated to be 33 Hz, so I thought I'…
Part Number: AMC1300 Other Parts Discussed in Thread: AMC-AMP-50A-EVM
Tool/software:
Hi team,
When AMC1300 is used in solar inverter phase current sensing, the SiC MOSFET is TO247-4 package, pls check below questions:
1. Should INN pin be connected…
Part Number: TAS5825MEVM Other Parts Discussed in Thread: TAS5822M Hi!
I am looking for a stereo power amp / speaker amp EVM that can take a digital audio input from a USB cable, connected to a Linux PC.
Actually the purpose of the stereo amp is to…
Hi Sapana,
425Arms with a 500uOhm shunt is 90.3W, which for many applications is beyond tolerable heat dissipation. I would expect most applications to instead use a smaller value shunt, perhaps 50uOhm which would then pair nicely with the 50mV input…