Taras,
Send on the completed quickstart calculator file (with the correct MOSFET parameters entered) as well as the schematic and layout. I notice you have a ton of ringing on the SW node voltage. Is it possible to use 80V instead of 100V FETs for…
Hi Suren,
Yes it's AMC package. We are using ti-linux kernel 6.1y release 9.2.1.
In EVM its working.
Only observation is we get
Pawan S said: Aplay command exits after playing audio in EVM but in our board after aplay ,it's stuck and need to give…
Can you check the following voltage rails while performing the tests:
Processor Voltage Rails:
VDDS_DDR = VDDS_DDR_C = 1.2V
VDDA_PLL0 = 1.8V (AM62x)
VDDA_DDR_PLL0 = VDD_CORE = 0.75 or 0.85V (AM62 AMC package only)
Memory voltage rails…
Hi Frank,
So, there is no modification needed on the hardware of TSWDC155EVM. The customer's jumper settings are fine. However, they do need to power on the board via the EVM before they can communicate via JTAG. To power on, on the GUI, press the …
Hi Jim,
Thanks for your patience.
I want to confirm if you have a custom board or the EVM board from TI?
So currently I have SK-AM62B-P1 which is basically ALW package, once I get my hands on AMC package I will test it out with SK-LP example as…
I've also now managed to make the EVM also pull this ~20A of current periodically. Note that it doesn't always do it, just sometimes. And sometimes you have to discharge the output caps all the way before turning the VAC supply on.
Configurations that…
Can you confirm you can access that compiler from the command line, like this?
a0797059@dasso:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_00_01_03
$ export PATH=/home/a0797059/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_00_01_03/linux-devkit…
Hi Jagan, The device is capable in theory. It will be extremely hard to realize this design and we advise against it. As I mentioned, this device is not meant to handle 500W. If you choose to go that route you will encounter complications. Additionally…
Hi,
Is this for an automotive or non-automotive application? We have multiple TPS65219 part numbers that are pre-configured to support different application requirements and use cases. TPS65219 20 supports automotive applications using AM62x-Q1 (17x17mm…
Hi Dave,
Butters said: I'm guessing at this point that you either didn't have the time to try that yet, or it didn't make a difference for you -- but if you have any updates, please let me know.
Yes, you have guessed correctly. I was not able to make…