Part Number: AMC0311R
I am looking for a SPICE model for the AMC0311R for simulation purposes.
I have checked the TI's website and available resources but have not been able to locate a suitable model.
I would greatly appreciate your assistance…
Part Number: AMC0311R-Q1 Dear TI experts,
My customer made their schematic using AMC0311RQDWVRQ1. Could you review this schematic?
+HV = 1000V
Applied 5V full scale. Customer will use the range 0V ~ 4.5V.
Best regards,
Chase
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311R Hello,
For AMC0311R-Q1 the recommeded conditions are given as -
But the absolute max ratings are as below -
So as per above absolute limit of upto 7V, can I apply 4.81V to the…
Part Number: AMC0311R Hi TI Team,
Do I need to tie the SNSN pin to GND2, or can a voltage offset be applied to this pin? In my application, the voltage between SNSN and GND2 would be up to 2 V, and the voltage between INP and SNSN would also be up to…
Part Number: AMC0311R-Q1 Hi Team
Now we develop a OBC product, and we use the AMC0311R-Q1 to detect the voltage of the High voltage Bat. From the datasheet , i get that the Nonlinearity of VINP = 0.25V to 2.25V is 0.08% max.
But it is not the max…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311R , TLV9001 , AMC0311D , AMC0311S , ISOTMP35R
Hello,
In AMC0311R-Q1 datasheet, the clipping voltage = Nominal analog input voltage.
But, as per below equation on page 20 of datasheet…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC1311 Hi team,
My customer is evaluating the impact to isolated sensing secondary supply overvoltage because of the power IC failure. Could you please kindly help suggest the expected device…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311S , AMC1311 , AMC1351 , AMC0311R Tool/software: Dear team,
My customer wants to measure automotive 12V-Batt voltage with isolated manner because the system is hot-side MCU configuration…
Part Number: AMC1311 Other Parts Discussed in Thread: AMC0311D , AMC0311R , AMC0311S , Hello,
In the circuit below, at the output of the MFB filter I observe 20mVpp 623kHz noise. I suspect it comes from the chopper in AMC1311B and the differential filter…
Hi,
Good Day!
As you suggested the Output of AMC0311R will be upto Vref value. In our case we connected Vref pin to VDD pin (3.3V) because we are not using external Vref. For ADC ADS7253 we using 2.5V internal Vref.
We are not sure whether we…