Hello,
We are using the AMC1035.
We use modulator mode 0
Additionally, it is worth to mention that we don't see invalid conversion results even when this modulator failure occurs. The results are very precise and undisturbed.
Kind regards
Seb…
Hi Ray,
1. The AMC1035 EVM is designed to meet the IPC-D-275 standard. The same should be true for all of our EVMs.
2. The substrate used is FR-4.
3. No conformal coating is used on the AMC1035EVM. There is only LPI solder mask.
Regards,
Aaron Estr…
Part Number: TIDA-00914 Other Parts Discussed in Thread: TMS320F28379D , AMC1306M25 , AMC1306M05 , AMC3306M05 , AMC3306M25 , INA240 , INA241A , AMC1035 , ADS7042 , LMG1210 , ISO6760 My customer is considering a new generation of servo driver design based on the…
Thanks for the schematic!
If you look closely at the AMC1035 and AMC1210 timings (the setup and hold for the AMC1210 and hold/delay times for the AMC1035), you'll see that you are on the edge of violating the hold time for the filter. With the data…
Part Number: AMC1300 Other Parts Discussed in Thread: AMC1311 , AMC1035 My customer needs to measure 1000V re-enforced. Currently they look at AMC1300 plus resistor divider. But it is still too expensive. Is there any cheaper solution.
BR Josef
Part Number: TMS320F280049 Other Parts Discussed in Thread: AMC1035 , Tool/software: Code Composer Studio I am using SDFM module in TMS320F280049 with AMC1035. I would like to have synchronized measurement with PWM1 module which generates signal at 50kHz…
Part Number: TMS320F280041 Other Parts Discussed in Thread: AMC1035 , AMC1106E05 Hi I have a project using TMS320F280041 and two Sigma-Delta Modulators (AMC1035 and AMC1106E05). The AMC1035 is configured for Manchester mode. Both are clocked from PWM generated…
Hi Fred, If this is the primary thing they're looking to evaluate on the C2000, then I'd use the LaunchPad of the device that they are most interested in. (for example: LAUNCHXL-F280049C) The controlCARD is another option. It will bring more of…
Part Number: AMC1306M05 Other Parts Discussed in Thread: AMC1035 , ADS1203 , ADS1202 Is there a const-sensitive,non-isolated version available?
Just w/o the isolator integrated?