Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , UCC28711 Tool/software: Hello:
Pl take a look at the attached sch : it has AMC1200 amp in a very std way of isolated current sensing.
In the application, voltage across the current…
Part Number: AMC1200 Tool/software: Hi
i am using a acm1200 device to monitor a supply voltage. All is well at ambient, but below -20 get errors (dips) even though the supply is driven from a PSU.
as this a controlling a motor, noise may be the issue…
Part Number: AMC1200 Other Parts Discussed in Thread: AMC1311 Hi,
1.We are facing a issue while using this configuration actually when we apply 565V DC at VDC_IN we are getting 0.1782 across R38, But as per calculation it should be 0.188 now we are…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC1351 , AMC3330 , ISO224 Tool/software: Hello All, I'm looking for a drop in replacement for the AMC1200-Q1 IC. Currently, this IC is being used to isolate two ground planes, it also…
Part Number: AMC1200 Other Parts Discussed in Thread: AMC1311 , , TS321 I am using AMC1200BDWVR amplifier for measring voltage of DC bus, but now i am facing one problem when the voltage athe VDC_IN is zero the output is showing 600mv
we have connected…
Part Number: AMC1200 Tool/software: Hi,
we are using the amc1200SDUBR and having issues at between -30 and -40C. the devices are tin dipped before being fitted to the board and the boards are formally coated to to prevent moisture issues. The system…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Tool/software: Hello:
Pl take a look at the attached schematic.
A signal of 100mV, 1kHz is applied to the inputs of AMC1200-Q1 through balanced RC filters.
U2 amp is biased on the…
Part Number: AMC1200 Tool/software: I am using the following design to measure AC current:
The resistive values in the differential amplifier circuit are 15k, hence the gain is G = 1. This circuit should work according to the application notes…
Part Number: AMC1200 Other Parts Discussed in Thread: AMC3301 Tool/software: Hello, I am designing the Power Monitoring Device for AC220V. In the voltage measuring part, I need isolation. So, I want to use AMC1200, a device for a fully Differential Isolation…