Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , UCC28711 Tool/software: Hello:
Pl take a look at the attached sch : it has AMC1200 amp in a very std way of isolated current sensing.
In the application, voltage across the current…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC1351 , AMC3330 , ISO224 Tool/software: Hello All, I'm looking for a drop in replacement for the AMC1200-Q1 IC. Currently, this IC is being used to isolate two ground planes, it also…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Tool/software: Hello:
Pl take a look at the attached schematic.
A signal of 100mV, 1kHz is applied to the inputs of AMC1200-Q1 through balanced RC filters.
U2 amp is biased on the…
Part Number: AMC1200-Q1
Tool/software:
Hello Team,
Customer found the 1pcs device failure return as the differential output voltage is abnormal in production line. and the unit had been analysis with FA( QEM-CCR-2503-00012) before. however the…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC3311 Tool/software: Hello,
We're trying to design a circuit to measure an isolated 0 to approx +40VDC isolated voltage, using the AMC1200-Q1 ( see below). As you can see, we have 100k/348…
Part Number: AMC1200-Q1
Tool/software:
I have design two HV monitoring block for input (LV : 400V )and output voltage (HV: 800V) monitoring of non isolated HV DCDC converter using this IC for max 1250V (Both ICs common power supply rail VDD_5V_ISO…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3301 , AMC1300 Dear support,
I use AMC1200 to do current sensing in my design.
The input power of my design is DC 48V to 160V.
VDD1 & VDD2 = 5V, magnitude of current to measured…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC1200EVM , AMC3301 , INA236 Dear support,
I plan to use TI above 2 TI IC for current & voltage sensing in my design.
Can you help me to check with TI whether my preliminary circuit…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Hello TI Team,
I am planning to AMC1200-Q1 for AC Voltage Sense. Does AMC1200-Q1 support for AC voltage Sense?
If yes then,
Can you explore me the point VINN and GND1 is short…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , OPA350 I designed the measuring circuit with AMC1200. At input I have a peak voltage 200 mV AC. The oscillograms of the inoutmeasured exactly at the inputs of AMC1200:
Unfortunately…