Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Hi
I want to know if AMC1200 has the power sequence requirement for high side supply voltage and low side supply voltage. if high side goes first, does this cause latch-up problem?
thanks…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , ISO224 Hello,
I will use AMC1200Q1 to supply proper voltage to ADC of TI 320F2837D DSP. First , I measure the 110V rms voltage using LEM LV25-P, then I will connect AMC1200Q1 to output of…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC1211-Q1 , AMC1311 We like to use AM1200 for voltage monitor, please help to Description different for AMC1200 vs AMC1200B vs AMC1200-Q1 ,thanks !
Part Number: AMC1200-Q1 What's the threshold voltage for the VDD1 and VDD2.
In the d/s, the VDD1 range is from 4.5V to 5.5V. What's the threshold voltage of the VDD1? For example: 3V or 4V??
Since customer finding current sensing problem with…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Hi Support team,
I connected LEM LV25P voltage sensor and AMC1200Q1 for voltage measurement.
I have two power supplies each has 4 channels, one DC power supply is for LV25P (VCC1, VCC2, GND1…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Dear TI team: My customer used AMC1200-Q1 in PTC product. When they test the EMC RS found AMC1200-Q1 failure.
The RS test frequency band is 1GHz-3GHz. At the beginning of the test, the…
Other Parts Discussed in Thread: AMC1200-Q1 , AMC1300B-Q1 , AMC1200 , AMC3330 , AMC1350 Hi team,
Could you recommend current sensing IC for output below?
This is AC output, so isolated device should be needed.
Total is 10ch. It doesn't have to be 10ch at…
Part Number: LM5158-Q1 Other Parts Discussed in Thread: LM5158 , AMC1200
Tool/software:
Hi TI Team,
I am planning to use the LM5158-Q1 for a POE application to boost the voltage from 40-50Vin to 52Vout/1A. I have the following queries:
The datasheet…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , , AMC1301-Q1 , AMC1311-Q1 Hi
in AMC1200 datasheet, the absolute max ratings, max Junction temperature Tj is 150 degree C.
but in recommended operating conditions, max operating ambient temperature…