Part Number: AMC1301 Other Parts Discussed in Thread: AMC1351 Hi guys.
I want to design isolated voltage to 4-20mA converter. I am using MCU with DAC. I designed the schematic using AMC1301 and XTR11.
DAC value max ==> 3.3V. Circuit if working fine…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC3330 Tool/software:
I’m using the AMC1301 in my design—does the current layout have any issues? Are there any improvements I can make? Also, are VINP and VINN impedance-matched in this design…
Part Number: AMC1301 Dear Sir or Madam,
We use the AMC1301DWVR component in our products. For this component, there is a PCN Notification # 20260327000.0. My questions:
Has the functionality changed?
Have the isolation properties changed?
…
Part Number: AMC1301 Tool/software: Hello,
As per figure 6-15 in the datasheet, it looks like we can "tune" the input bias current by applying a common mode voltage (Ibb is null at Vcm = 2V).
However, there is no indication of the sensitivity of the…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC3301 , AMC0300D ,
Hi TI Experts,
I am currently designing a current shunt sensor and was checking the capability of my circuit to reject common mode. As I understand, CMRR is defined by 20Log…
Part Number: AMC1301-Q1 Hi Texas, AMC1301QDWVRQ1 for this part number can i get the phase versus response frequency where the input ac signal I gave is very different from the output it had phase difference and the required one is not plotted in datasheet…
Part Number: AMC1301 Tool/software: Hi I am using this part
Can you please let me know what will be MAX GND voltage difference between input GND1 and GND2 connections that we can use.
Thanks
Part Number: AMC1301 Other Parts Discussed in Thread: OPA320 , , AMC1300 , AMC1302 , AMC3302 Tool/software: Hi,
I am trying to design a shunt based DC current sensing circuit using a isolator AMC1301 and OPA320.
There are similar current sensing circuits…
Part Number: AMC1301 Other Parts Discussed in Thread: TINA-TI , ISO224 , AMC3330 , AMC1350
Tool/software:
The attached diagram is the circuit diagram and simulation diagram of AMC1301, with an input DC voltage of 328V. Is the circuit on my simulation…
Part Number: AMC1301 Tool/software: Hi team,
My customer is using AMC1301 for 3-phase motor current sensing. Issue is that there is no signal output on the output end.
They use 5V power supply on primary side and secondary side. Shunt resistor is…