Part Number: AMC1301 Hello all, Please I would like to know if a technical documentation exists, explaining tests of AMC1301 datasheet. Indeed, for example, SNR is @ fin = 1kHz and BW = 10 kHz. I understand I have to input a sinus wave of 1kHz , and i have…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 In AMC1301 datasheet, there is comment for input filter components design.
it's said the C6 C5 must be 10-20 times lower than C5.
could you specify the reason behind. In my circuit, seems…
Part Number: AMC1301
Hi, Support Team
We have a question if VRb=0V, and we find output offset have 0.6v? is normal?
schematic:
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: LM5164 , AMC1301 The schematic represents an Isolation Monitoring Device(IMD) for a HV System specifically for EV Application.
The Voltage rating of the Battery Pack is 400V when fully charged.
The…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC1350 , AMC3330 Hello,
I am designing a isolated voltage sensor. I want to use the AMC1301 isolated op-amp IC. I designed a section, but I am not sure if my connections are right or not.
The voltage…
Part Number: TIDA-00366 Other Parts Discussed in Thread: OPA320 , , AMC1301 , TLC372 , LM393 , OPA2350 HI everyone! I would be happy if you take a time and answer these questions :
Q1: In "TIDA-00366 => TIDUBX1B.PDF => page 17 => Figure 13. Differential-to…
Part Number: AMC1301 Hi team,
Do you have the min and max value for input resistance? for the device itself, will this value be changed over time? In my customer application, we found a issue that the voltage sample changes a little over time for a fixed…
Part Number: AMC1301-Q1 Hello TI's experts,
I'e built the schematics below based on TIDUBV1A.
Scope results : signal injected on first stage preamplifier (by removing both R19 & R28). The blue is the signal coming from Arb waveform generator…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC3302 , AMC3301 , AMC1302
Schematic specification 28V , 300A
1.Is there a solution to the resistor heating problem?
2.Is there a replacement for the AMC1301?
Part Number: AMC1301 Dear Sir or Madam,
Could you inform me about terminal finish f or each one of the parts AMC1301SDWV & AMC1301SDWVR . Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Also, could you tell…