Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 , AMC1300 , AMC3330 , AMC1311 Dear Sir,
Please find the Schematic of High Voltage Measurement and High Voltage Isolation Schematic.
This schematic is based on TI Application notes.
Kindly review…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC1300 The AMC1301 has a High-Side (shunt side) and a Low-Side (MCU side). The device basically does an "Analog -> Digital -> Analog" conversion, all with Vin -> Vout delay of under 3.0[us].…
Part Number: AMC1411 Other Parts Discussed in Thread: AMC1301 ,
Hi all
My customer is currently using the AMC1301 for a project with 1000V working voltage.
They have now a new project with 1500V working voltage and are looking at the AMC1411 with wider…
Part Number: TIDM-1000 Other Parts Discussed in Thread: AMC1301 Hi,
Vout can reach 800V, V_ P is 400V, and the input of amc1301 is 400/3002.74*2.74=0.365v, which is beyond the input voltage range of amc1301. Even if Vout is 700V, the input of amc1301 is…
Part Number: AMC1301 Hi Team, I am using the TIDA-1606 inverter (10 kW, bidirectional three-phase three-level (T-type)) and I have a problem with the data from the AMC1301 sigma-delta converter for grid current measurement. I use a voltage source on the…
Part Number: AMC1301 Other Parts Discussed in Thread: OPA320 , TIDA-01513 When measuring high voltage using the aMC1301, a lot of noise is added to the input side. Is there any solution for it?
I am attaching the schematic and scope image.
measure point…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC1300 Hey Team,
Could you help me out on getting some information on a TI part. For the AMC1301, the datasheet shows that it has short circuit protection on the output is up to +/- 13mA and an output…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC1300 Hi TI,
I am working on AC Voltage and Current sense circuit for that I am referring AMC1301DWVR part which is not available. I checked alternate part no AMC1300 and AMC1300B both are not available…
Part Number: AMC1301 Other Parts Discussed in Thread: TIDA-01513 , AMC1300 , AMC3330 , AMC1350 , Hi team,
I help my customer to post a question.
"I want to get some technical assist for TIDA-01513 High voltage measurement,in this circuit i think GNDi and HV_NEG…
Part Number: AMC1301 Other Parts Discussed in Thread: AMC1300 Hi Team,
AMC1301's signal delay time is too long for my customer's application, do we have any isolated amplifier with lower delay time?
Thanks.
Regards,