Part Number: AMC1301-Q1 Hi team,
Could you advise the device operation at below missing power supply scenario?
1. Missing(Open) VDD1
2. Missing(Open) GND1
3. Missing(Open) VDD2
4. Missing(Open) GND2
I think in the case of #1 and #2, VOUTP…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 , ISO124 I want to use AMC1301-Q1 to isolate analog signal.The input range of AMC1301-Q1 is ±250mV,and fixed-gain is 8.2. But table 6.1 indicate the range of VINP is (GND1-6) to (VDD1+0…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 Hello
Please guide me through this query.
I am using AMC1301-Q1 for motor current sensing using shunt resistor. The datasheet of AMC1301 suggests inherent Vcmout = 1.44 V. But according…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 , OPA365 I was testing the part AMC1301 in my lab using in inverter application, found one strange thing, the gain (8.2) is in Tina simulation and when applying a DC signal or a signal till…
Hi Peter,
The first page of the AMC1301-Q1 datasheet is just showing a typical application, which depicts (for example) one phase of a three-phase motor drive. You don't have to add FETs or gate drivers to use the AMC1301. If this is a voltage measuring…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 , I have desided to use amc1301 IC for bms current measurement. In BMS max current to measure is 120A. Whether this is suitable for such a high current measurement?
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 Due to high current, the application will use two equal sense resistors. I need to measure both resistor voltages as the current split might be 49%/51% (or similar)
Using just one LMC1301…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 Could you confirm that in AMC1301-Q1 datasheet (pag 12, fig 24) Voutp and Voutn are opposite and they should be exchanged (that is, Voutp and Voutn are the same as AMC1301 Rev.E datasheet…
Part Number: AMC1300B-Q1 Other Parts Discussed in Thread: AMC1301-Q1 Tool/software: Hello,
I'm interested by the AMC1300B-Q1 but also by the AMC1301-Q1. Before to make a choice, is it possible to know if it is the same chip in the amplifier ?
Also…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: AMC1301 Hi,
We've designed a dual scale current measurement board which uses two AMC1301 to measure the voltage drop across a 100R and a 0R2 shunt resistors placed in series. The AMC1301 associated…