Part Number: AMC1302 Hello,
We are investigating using the AMC1302. There is a 1µs to 1.5µs delay between an input step reaching 50% of full scale and the output voltage rising to 10% of full scale.
Is this purely due to the amplifiers in the IC coming…
Part Number: AMC1302 Dear TI,
I am going to buid an inverter prototype with 1500V DC-link voltage. The output voltage is 690V (L-L rms). I am wondering if AMC1302 can be used to measure the current or voltage in this situation? I see in the datasheet…
Part Number: AMC1302 Other Parts Discussed in Thread: AMC3302 Hi,
What is the maximum voltage of HV+ that can be used, when using AMC1302 in phase current measurement for BLDC motor current sensing application.
Can we use 20Khz PWM switching.
regards…
Part Number: AMC1302 Other Parts Discussed in Thread: AMC1300 Hi,
I am working on the current detection problem of AC motor. The shunt resistor scheme is used to detect ac current. There are two isolated amplifiers that I can select, AMC1300B and AMC1302…
Hi Kishore,
This should be fine. The bandwidth of the AMC1300B is 250 kHz (min), 310 kHz (typ), plenty of margin compared to your maximum frequency of 140kHz.
Part Number: AMC1302 Other Parts Discussed in Thread: PSPICE-FOR-TI , TINA-TI Hello,
There is any way to include the model of AMC1302 to simulate it on PSPICE-FOR-TI? I have seen the 1301 but some characteristics are differents and I'm looking to…
Part Number: AMC1302 Hello,
We use the mentioned part in a 3x SiC-bridge configuration to measure the phase currents. On some ICs we measure a 600kHz oscillation in the output signal - it seems to be random over the phases and the units. Some units…
Part Number: AMC1302 Hello,
I am trying to implement a AC current sensor which has a variable frequency and can reach up to 250 KHz (shunt resistor is on the HIGH side). For that I am using AMC1302 as an isolation amplifier followed by a differential…
Part Number: AMC1302 Hello,
My customer has been using AMC1302 for current sensing. They have found AMC1302 output distortion when input is 20KHz, +/-40mV voltage signal. The gain of AMC1302 is 41. However, with the same schematic and parameter, the…