Part Number: AMC130M02 Good evening,
I was wondering is AMC130M02 can be used to measure voltage and current of the -50V rail? If not can you recommend one that can be used? Also a reference design for this application would be appreciated.
Thanks…
Part Number: AMC130M02 Other Parts Discussed in Thread: AMC131M03EVM Tool/software: I am using an AMC130M02 for an isolated power bus voltage and current measurement, but have so far had no luck in establishing solid communication with the device to configure…
Part Number: AMC130M02 Other Parts Discussed in Thread: AMC131M02 Tool/software: Hi,
we had trouble initializing the AMC130M02 according the procedure described in datasheet.
We should:
disable the CLKIN signal
do a long pulse on reset
wait…
Part Number: AMC130M02 SPI.xlsx
Tool/software:
Hi all,
1) About WREG command,
Can WREG command write only 1 register when n=0 is specified like RREG command?
My customer is guessing that WREG command only supports writing multiple registers…
Part Number: AMC130M02 Tool/software: Which of the isolated ADC have SPI interfaces? The selection table says "Serial CMOS" in the interface column for both SPI devices and devices with raw sigma-delta outputs.
Part Number: AMC130M02 Tool/software: Hello,
I'm thinking about specifing the AMC130M02 in our products systemdesign. From a Hardware point of view this looks like a good fit.
But are there are any further software drivers/middleware or libraries…
Part Number: AMC130M02 Tool/software: Hi all,
I would like to know clock requrirements of this device.
Since a clock cannot be supplied from a MCU, my customer is considering supplying a clock using a crystal oscillator.
EVM is equipped SiT8924…
Part Number: AMC130M02 Tool/software: Hi Team,
a general question concerning the GPO. The GPO on pin 6 is currently not used and thus, register GPO_DAT is set to (or left at) "0b" (=Output disabled). Since the GPO is a push/pull stage and the datasheet…
Part Number: AMC130M02 Tool/software: Hi All,
I would like to know how to convert single end to differential signal.
Is it possible to exchange information properly if I use AD2 fixed to GND? Or is there another good way?
Input voltage of AD1 and…
Part Number: AMC1302 Other Parts Discussed in Thread: ISO1212 , , AMC130M02 , AMC1300 , AMC3301 , AMC1350 , AMC3330 , TIDA-010960 Tool/software: Hi Team,
My customer would like to design a 240VAC input power detector. Max power is 1.8KW.
Could you…