Part Number: AMC1311 Other Parts Discussed in Thread: AMC3330 I am using AMC1311 for a sensor that was used to measure the power line. The low side of AMC1311 was fed into an adc pin to a TI microcontorller.
assume I use AC power line for input, 120v…
Part Number: AMC1311 Other Parts Discussed in Thread: TLV9002 , TLV9001 , AMC0211S , AMC0211R Hello,
I am working on a BLDC motor driver project and designing the battery voltage sensing circuit. The battery has a nominal voltage of 48V and a maximum…
Part Number: AMC1311-Q1 Dear TI experts,
My customer have a question about the specification of AMC1311-Q1.
I saw that the input range of AMC1311-Q1 is 2V(peak to peak).
And I saw the parameter below.
Does it mean that from 2.0V to 2.516V input…
Part Number: AMC1311 Hi Team,
Customer needs CB certification(Certification Bodies' Scheme), I cannot find it on ti.com, could you please help provide it? Thanks.
BRs,
Francis
Part Number: AMC1311 Other Parts Discussed in Thread: AMC3311 Hello E2E Experts,
Good day.
Using the AMC1311 board (which you had previously said you would support and recommend going forward in a medical application/if IEC-60601-1 clearance was needed…
Part Number: AMC1311 Other Parts Discussed in Thread: TINA-TI Hi, There is an AMC1311 example design for TINA-TI that uses the model witn a revision 1.2. Unfortunately the AMC1311 model for TINA-TI that is downloadable still has an older revision. 1)…
Part Number: AMC1311 Other Parts Discussed in Thread: UCC12050 Device: AMC1311BDWVR Datasheet: SBAS786C
We are designing a 4–20 mA current-loop input board using the AMC1311B.
The isolated high side is powered from a UCC12050 set to 5.0 V, so VDD1…
Part Number: AMC1311 Other Parts Discussed in Thread: ISO224 , AMC3330 , AMC1350 Hello E2E Experts,
I want to design an isolation barrier that isolate a 0-2V input signal. The signal could go 10% under and over range, so the signal that has to be reproduced…
Part Number: AMC1311 Other Parts Discussed in Thread: INA826 ,
Sr,No.
Manufacturer Part Code
Manufacturer Name
Discreption
Quantity
1
ISO7741DWR
Texas Instruments
ISO774x High-Speed, Robust-EMC Reinforced and Basic Quad-Channel…