Hi Frank,
Frank QIN said: While the datasheet recommendation series resistance is 10 Ohm, so what is our suggested best value range?
We will likely update the datasheet to increase that resistance value, since the the cutoff is higher than necessary and…
Part Number: AMC1311-Q1 hi expert
taking TCVOS as an example,
There is a comment(1) in datasheet.
do we use one standard deviation (sigma) or six standard deviation (sigma) to describe these parameters?
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC3330-Q1 , Hi Team,
Customer is design CAR OBC and using AMC1311-Q1 and AMC3330-Q1 for BAT voltage sense.
End customer request ASIL-B level for this function block. Do we have any reference design…
Part Number: AMC1311-Q1 Hi TI Expert,
We notice the VFAILSAFE(VOUTP - VOUTN) will be -2.6V if following condition is fulfilled.
Is there any way that we can keep the VOUTP-VOUTN as 0V even the VDD1 power is missing?
Or the only way is to disable the…
Part Number: AMC1311-Q1 Hello, Team,
The datasheet only specifies the failsafe differential output voltage V_FAILSAFE with a condition of VDD1. Also, 7.3.3 only mentions about VDD1 and SHTDN when this fail-safe output occurs.
Does this mean that VDD2…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 , Hello team,
My customer is using AMC1311.
During their test, the input terminal (Vin) of AMC1311 may exceed 2V, almost 2.15V. However, after testing, there was no problem at all temperature…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 Hi Expert
Do we have wafer probing for the component of AMC1311B-DWVQ1?
This component can not be used if there ’ s no wafer probing in our system.
If not, do we have alternative for…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 AMC1311 EMC issues:
We find EMC RE issues when only enable TI-AMC 1311, and the noise gap is 30Mhz(200-900Mhz), please help me
Confirm this oscillator frequency and do we have some solution…
Part Number: TPSI3050-Q1 Other Parts Discussed in Thread: AMC1311 , TPSI3050 Hello,
We are working on a board with a 400V power input. We have an isolated 5V section to power our MCU and a few other LV Circuits. We need to monitor the voltage of our supply…
Part Number: TPSI3050-Q1 Other Parts Discussed in Thread: AMC1311 , TPSI3050 , Hello,
We are working on a board with a 400V power input. We have an isolated 5V section to power our MCU and a few other LV Circuits. We need to monitor the voltage of our supply…