Part Number: AMC1350-Q1 Other Parts Discussed in Thread: AMC1350 Hi Expert,
Q1:Can AMC1350 sample negative voltage.For example,INN connect to GND1,INP is -3V.
From above typical application,we can see when INP-INN is -5V,the absolute voltage of…
Part Number: AMC1350 Tool/software:
Generally, when using differential signals as inputs, a bias voltage is required, such as a bias voltage of 0, in order to produce an output. Why does AMC1350 differential signal still have output without bias voltage…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1351
Tool/software:
Dear TI
I am an engineer developing inverter converter system from several kW to several tens of kW. And I am designing bipolar signal sensing and unipolar signal sensing…
Part Number: AMC1350 Tool/software:
Why is the output waveform like this when there is no signal added and only input(VDD1) and output(VDD2) power supply?
After superimposing the input signal, there is no change before and after。
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1351 , Tool/software: Hi team
Could you tell the differences between AMC1351DWVR and AMC1350DWVR?
It seems that there are diffrences about input voltage range and output voltage range as below…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1300 Tool/software: Greetings, I am using AMC 1350 and AMC1300 for sensing current and voltages and I am reading more than max rated offset errors in multiple instances. One of AMC1350 has an offset…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1351 , AMC3330
Tool/software:
Hi All,
I am considering using AMC1350 ( datasheet ) for the three-phase AC line-to-line measurements. It has ±5V input, ideal for AC signals,
According to…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1400 Hi, I am wondering why all the Ti's isolated amplifiers have net gain of 2v (i.e. AMC1400 0.25V input, fixed gain of 8V/V =>2V outs/ AMC1350 +/-5V input, fixed gain 0.4v/v=>2) The ADC I am…
Part Number: AMC1350 Hi,
I'm looking for an isolation amplifier for a 2Vpp 250KHz signal which appears to be challenging to find. The closest I could find is the AMC1350 and I have the following questions:
1) The frequency of interest in my application…