Part Number: AMC1351-Q1 Hi,
I want to use AMC1351Q1 in order to read an analog sensor data. The voltage range od the sensor is 0-5V. Is possible to read the sensor voltage in this range when I supply VDD1 of the AMC1351Q1 with 3.3 V supply?
Part Number: AMC1351-Q1 Tool/software: Hi,
Could you please provide information on the following items regarding the AMC1351QDWVRQ1?
・Humidity resistance
・Vibration resistance
・Shock resistance
Best Regards,
Nishie
Part Number: AMC1351-Q1 Other Parts Discussed in Thread: AMC1350 , AMC1351 Dear TI experts,
My customer asked Pspice model of AMC1351-Q1.
Could you check this file?
Best regards,
Chase
Part Number: AMC1351-Q1 Other Parts Discussed in Thread: TLV313-Q1 Tool/software: I am designing a circuit to detect voltage with a detection range of 800V through isolation using the AMC1351-Q1.
I am considering the circuit constants using the "IsolatedAmplifierVoltageSensingExcelCalculatorRevC…
Part Number: AMC1351-Q1 Tool/software: Section 8.2.2.1 (snippet below) talks about the design requirements for the input filter to the isolator.
Is this saying to design the input filter such that the cutoff frequency is >2MHz?
Does the input…
Part Number: AMC1351-Q1 Other Parts Discussed in Thread: AMC1351 Hello,
I'm using this isolated amplifier AMC1351-Q1 to monitor a voltage busbar (1200Vdc max).
I have included a voltage follower between the divisor resistors and the input pin of…
Part Number: AMC1351-Q1 Hello team,
Good morning.
For the high voltage DC measurement we are using AMC1351-Q1 (single ended input and differential output). To perform the Mote-Carlo LTspice simulations for the worst case circuit analysis we have used…
Part Number: AMC1351-Q1 Other Parts Discussed in Thread: AMC1351 , AMC1311 Hi team,
What is wider input voltage (0..5V) benefit compared with narrower input range (0..2V)?
AMC1351-Q1 and AMC1311B-Q1 looks similar but different input voltage range…
Part Number: AMC0311S Other Parts Discussed in Thread: AMC1351-Q1 Team,
Could you help to comment on the p2p compatible device with ADuM4195-1 device? It looks AMC0311S is not exact the same device, right?
Here's current layout placement of ADuM4195…
Part Number: INA241A-Q1 Other Parts Discussed in Thread: AMC1351-Q1 , OPA2188 , INA241A , TLV387 Hello E2E Experts,
I have several elementary questions about offset voltage in a current-sense amplifier:
Question 1: If I compensate the offset voltage…