Part Number: AMC3302-Q1 Other Parts Discussed in Thread: AMC3330-Q1 , , AMC3330 Tool/software:
Hello Team
I have attached the images from datasheets of AMC3330-Q1 & AMC3302-Q1 to understand about the difference in the differential input resistance…
Part Number: AMC3302-Q1 Other Parts Discussed in Thread: AMC3302 , TLV316 Tool/software: Hi every one,
Recently, when we used AMC3302-Q1 and TLV316QDBVRQ1, we found that when the current rise slope is below 20A/us, the output voltage is…
Part Number: AMC3302-Q1 Other Parts Discussed in Thread: AMC3302 Tool/software: Hello, when we tested the 3302 module, we found that the jitter on the measurement side will cause a high-frequency voltage jitter of 3MHz ±7.8V about 8us at both ends of…
Part Number: AMC3302-Q1 hi ,
We're using the IC in situations where short circuit is likely to encounter. Shunt resistors are resistive at low frequencies but they pose bandwidth limitation at high frequency because of the parasitic inductance.
…
Part Number: AMC3302-Q1 Other Parts Discussed in Thread: AMC23C10 Tool/software: I have to build a board to monitor the precharge of an inverter with galvanical isolation, and I was wondering if it was possible using this IC, the idea would be to connect…
Part Number: AMC3302-Q1 hi Team ,
The DIAG pin is actively pulled low if:
• The low-side does not receive data from the high-side (for example, because of a loss of power on the high side).
• The high-side DC/DC output voltage (DCDC_OUT) or the…
Part Number: AMC3302-Q1 Other Parts Discussed in Thread: ADS131B02-Q1 , ADS131B04-Q1 , ADS131B26-Q1 We are trying to design an isolated current measurement design based on a shunt measurement principle for high battery charge and discharge currents. The…
Part Number: AMC3302-Q1 Other Parts Discussed in Thread: AMC3302 There’re several questions shown as below:
The maximum current of battery pack is above 1100A while the current shunt resistor used is 50uΩ. Howerver, the maximum input of AMC3302-Q1…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC3302 , AMC1311 , TLV6001 Hello Smith,
I have simulated both the isolated voltage sensing & Isolated current sensing using AMC1311 & AMC3302 respectively. I have added both files.
Kindly…