Part Number: AMC3306M05 Dear forum members.
Could you please comment on the nominal and maximum current sinking capabilities of the DIAG pin.
In short how much current could be sunk and still maintain typical TTL/CMOS levels at a supply voltage of…
Part Number: AMC3306M05 Other Parts Discussed in Thread: AMC3302 , AMC3301 Hi Experts,
While selecting components, I got to read up on using this IC to measure bi-directional currents. But I have a doubt on seeing this application circuit.
Since…
Part Number: AMC3306M05 Hi,
Would you please tell me what is the analog input bandwidth of AMC3306M05 which is not listed in the datasheet? (For the similar parts AMC1306 and AMC1303 I can find their input bandwidth as 800 kHz in the datasheets).…
Part Number: TMS320F28388D Other Parts Discussed in Thread: AMC3306M05 , Hi,
Holding time of AMC3306M05 is min 3.5ns.
But TMS320F28388D support only mode 0 at SDFM and it means data read at rising edge.
Could you let me know 3.5ns from rising edge…
Part Number: TMS320F28379D Other Parts Discussed in Thread: AMC3306M05 , LMK1C1103 Hi,
We are evaluating the AMC3306M05 and we seem to be having issues with noise in our control loop when it is recovered from the TMS320F28379D MCU at certain duty cycles…
Part Number: LMK1C1103 Other Parts Discussed in Thread: TMS320F28379D , LMK1C1104EVM , AMC3306M05 , LMK1C1104 , What is the proper termination for signal integrity for the LMK1C1103PWR if I were going to route it out to the AMC3306 and use that same signal…
Part Number: INA219 Other Parts Discussed in Thread: AMC0311D-Q1 , INA260 , INA226 , ISOW7842 , AMC3306M25 , AMC3306M05 , TIDA-00313 Tool/software: Dear TI, as always thanks a lot for your great products and namely the current and voltage sensors line…
Hi Sam,
The low noise and high bandwidth are difficult requirements for an isolated system to meet. There is still one more magnetic solution you can explore, the DRV421, which is capable of meeting these requirements:
The DRV421 is not a hall sensor…
Hey Ismail,
No, that won't work because if the grounds are different then you don't know the potential difference between the two. For example, even though the battery is at -30V compared to its ground, it may not be within limit of the INA compared…
Hi Samiha,
1. Can it be interfaced on SPI or uart interface with MCU?
2. Have to measure 1000Vdc & 300A via shunt resistor
a) For voltage sensing , found that https://www.ti.com/product/AMC3336 has inbuilt dc-dc also, so simplifies design, so can…