Part Number: ANALOG-ENGINEER-CALC I downloaded ANALOG-ENGINEER-CALC after the install is indicates a newer version is available. I download and install again and get the same message.
From the webpage; I fill in the required information (name etc), the…
Part Number: ANALOG-ENGINEER-CALC Hi
There is a problem in version 1.6.0 with the data when the regional settings is not set to US.
More specifically, when the decimal symbol is a "comma", the program looks like this:
and after setting "dot…
Part Number: INA333 Hello,
I am looking at the Analog Engineer's Calculator with my customer on the INA Vcm vs Vout tab for the INA333 as the selected component. The outputs are limited to 4.7V max and - 0.3V min with 5V V+ and 0V V- with a 2.5V reference…
Part Number: INA321 I am using the INA321E, powered by a single ended 3.3V supply. I intend to apply a small differential signal at the inputs (~1mV) biased by a common mode voltage, centered within the allowable input common mode range.
According to…
Fresh installation in Windows 10, when selecting the "vcm vs vout" calculator a message window with a "Supply or Ref voltage out of Range" warning appears, and the "Select INA" list is empty (cannot select amplifier).
This…
Part Number: TSV912 I'm trying to work through the example shown in the "Analog Engineers Circuit - Non-inverting op amp with inverting positive reference voltage", document SBOA262A.
Starting in step 3 on page 2, where does the 1MΩ come…
I installed the Analog Engineers Calculator on one of my Win10 desktops (I already have it running on two other win10 machines with no issues). When I launched it, and opened the screen for INA VCM vs Vout, I got the following dialog box.
indicating…
When I run this tool with 7.5vdc in and 3.3vdc out, i get r1=140, r2=110 with an error of 0%.
It appears to me that the tool is trying to get the absolute least error values for r1 and r2
However, like in this case, the total current is 30ma at 7.5vdc…
Part Number: ANALOG-ENGINEER-CALC Hi team,
The customer wants to confirm if ANALOG-ENGINEER-CALC can be used for free. After downloading, NS general tool is also included. Including those software, all software package are for free to use ANALOG-ENGINEER…