Part Number: J721EXCPXEVM Hi Team,
I am attempting to boot my J721E EVM (Common Processor Board Rev A, SOM Rev A) from the onboard eMMC (MMC0).
Problem: When configured for eMMC boot, the UART console remains completely blank. No "CCC" characters…
Part Number: AM6442 Tool/software: Hi,
SD Card (ScanDisk) flash with image tisdk-default-image-am64xx-evm.wic using balenaEtcher.
Power to card vis USB-C ok as LED2, LED14 and LED16 are glowing light green.
Default DIP switch set to SD-Card…
Part Number: ADS131M08EVM Other Parts Discussed in Thread: ADS131M08 Hello,
I am using the ADS131M08EVM Eval Board and I'm getting an EVMEEPROM error when I try connecting to the ADS131M08 EVM software. It says to use the EEPROM Loader but I'm unsure…
Part Number: TPS65988EVM Other Parts Discussed in Thread: TPS65988 , TPS65987 My customer is testing our TPS65988EVM, wants to use one USB-C out to deliver eDP1.4 at 4 lane source capability (don't need USB3.0 SS data on that link). Can we provide a firmware…
Other Parts Discussed in Thread: BQSTUDIO BAT_SHUNT_04-0134_A-vis.pdf
Hi, I've attached the datasheet for our product battery shunt resistor. We use 2 in parallel for effective 0005 value @ 6W, our current from K-2 Energy LFP26650P can be > 80A.
We…
Other Parts Discussed in Thread: CC3100MODBOOST , CC3200MOD , CC3100MOD Hi,
Please help me with this questions below:
Dimensions of:
CC3100MODBOOST
CC3200MODLAUNCHXL
Flash Memory of the CC3100MOD/CC3200MOD – what is the minimal size…
Hi,
I wanted to share some test code that I did for myself, maybe someone else can find it interesting as well.
It is based on StarterWare v2.00.00.07 and was tested via JTAG emulator and run directly in DDR.
There is a ReadMe.txt in the attached…
Hi,BJ,
why dont you try with dump_stack to see where does the problem come form ?
i had tried to put it at _davinci_disp_disable_layer and see:
[<c008c5f4>] (dump_backtrace+0x0/0x114) from [<c039db50>] (dump_stack+0x18/0x1c) r7:c2001000 r6:00000000…
Hi Josh,
Thanks for the detailed input.
Couple of queries.
1) One confirmation require. All your input are applicable CC3300 MOD as well as CC3300. Please confirm.
CC3300 MOD is CC3300 IC + antenna + 40 MHz crystal as mentioned in block diagram…
Hi,
That shouldn't be the case. This hardware mod has been tried on our j784s4 EVMs and we are able to see the logs.
Can you confirm these are the only hardware modifications you made?
Regards, Tanmay