I know this is an old thread, but I just came across it and wanted to give an update that the TCAN4550-Q1 device could be used in order to achieve a CAN or CAN FD interface using the MSP430. It is a CAN controller + transceiver with SPI interface to support…
Hi Josel,
I can help you get this up and running. Can you provide me with a bit more information about your test setup?
Are you using a TCAN4550EVM or a BOOSTXL-CANFD-LIN board?
I am familiar with the Digilent Digital Discovery, are you using it to configure…
Kai,
Thanks for bringing this to E2E and happy to hear that the customer is evaluating TCAN4550-Q1.
1. Yes, the TCAN4550-Q1 does support CAN 2.0B.
2. Any MCU with a SPI module will work. We have starter code that was generated using a MSP430 variant,…
Hi Jonathan.
First of all. Thank you for your support.
You asked several observations and I carried out most of them.
1. You mentioned about wrong SCLK. And I also agree with you. So I added 200ohm serial register on SCLK (our PCB made by H/W team). As…
Part Number: PGA460PSM-EVM Other Parts Discussed in Thread: PGA460 , SN65HVDA100-Q1 , BOOSTXL-PGA460 Hi Sir
I am really confuse about OWU/OWI/LIN interface about PGA460.
Could you help to verify below question?
I saw the Interface type description of PGA460 …
I don't, but have you considered the TCAN4550-Q1 ? It is an SPI to CAN-FD with an integrated transceiver. There is already a booster pack with this device that will make it easy to develop code on the EK-TM4C123GXL launchpad.
http://www.ti.com/tool…
Part Number: TCAN4550EVM Other Parts Discussed in Thread: TCAN4550 , MSP430FR6989 , , BOOSTXL-CANFD-LIN Hi team
I want to configure the TCAN4550 into controller mode, send CAN frame via SPI interface and then check the output on GPO2. Can you tell me how…
Hi.. we have basic requirements like microcontroller should support CANFD and should be able to drive 45 LEDs using LIN.
Other requirements we want dual core.
20 input functions/signals shall be received fròm CAN-FD.
20 DIDs implementations.
We…
Part Number: TCAN4550 Other Parts Discussed in Thread: MSP430FR2476 Hi,
I communicate via CAN using 2 boostxl-tcanfd-lin EVM with 2 MSP430FR2476 with the FW demo available on TI.com, where I send simple messages using
- TCAN4x5x_MCAN_WriteTXBuffer(1, &header…
Dear Shu-Cheng LIN -
i know of the example that is available here: (this is the MSP432, there are other MCUs that support this same code example) - board with OPT3001 on it is BOOSTXL-BASSENSORS