I forgot to mention:
There's another option using the AM2x booster pack for brushless DC servo drive: https://www.ti.com/tool/BP-AM2BLDCSERVO , which has two RS485 half-duplex transceivers. We can use these to implement a full-duplex RS485 as needed…
Please note, we are told that you are trying to evaluate BISS , which requires the booster pack. The booster pack needs a 24V supply.
Your complete setup pictures are not in this post, so want to make sure about that.
SDK Example page link : AM243x…
Hi Sayali,
Thank you for your interest in TI's solutions for encoder interfaces.
I assume you have a single/multi-turn encoder with BISS-C interface? From am MCU either Sitara or C2000 support BiSS-C host.
Option 1: C2000 MCU The C2000 MCU provide…
Hello Mukul,
we have ordered LP-AM263 with BP-AM2BLDCSERVO , fortunately were able to cancel. Our final product will be motor drive supporting absolute all encoder and resolver protocols (serial, EnDat, BISS etc.). Support for industrial communications…
Part Number: LP-AM243 Other Parts Discussed in Thread: BP-AM2BLDCSERVO , , TIDEP-01032 , SYSCONFIG Hi TI experts,
I do have an EnDat 2.1 Absolute Motor Encoder, which I have hooked up to an AM243 Launchpad (LP-AM243) in conjunction with a BP-AM2BLDCSERVO…
Part Number: AM6442 Other Parts Discussed in Thread: TMDS243EVM , TMDS243DC01EVM , TMDS64DC01EVM , LP-AM243 , BP-AM2BLDCSERVO , BOOSTXL-IOLINKM-8 , TUSB320 , AM625 , AM62P-Q1 , TUSB321
Hi TI Experts,
I have the below queries regarding implementation…
Hi Divyaa,
Couple comments to help in your seleciton:
AM243x max clock speed is 800MHz but there are multiple core options
AM243x does not supoprt SGMII, but does supoprt RGMII
There are leaded pacakge options.
Please see attached background…
Hi,
Please see attached details on the AM243x with PROFINET support. Do you have local sales support?
AM243x Device option "F" incudes TI software supporting PROFINET.
2134.AM243x_Overview.pdf
Best regards,
Mike