Part Number: TDA4VL-Q1 Other Parts Discussed in Thread: TDA4VL Hi experts,
We make a customized TDA4VL board. In this board, we keep the DP0 port, and remove DP1 port, panel & bridge. Some code from SDK were modified but the DP0 port can't work in both…
Hi Ling,
I'll paste my generated code below. I'm expecting my first button to use TX pin CAP1.2 (connector C7) and RX pin CAP1.0 (connector C5).
It looks like it lines up to me, but I must be missing something. I probed every pin on the connector…
Hi Manikanta,
Unfortunately I am not at work now, but here is what I can give you now:
UCC256403 Design 25 Jan 2023.xlsx
The VCR lower capacitor value is 8.2nF and the VCR upper cap value (which is presently not fitted) is 68pF.
Resistor on FB…
Hi Cristian, I don't have answers for all of these right now but I'll give this a shot. Cristian Bogus said: 1. Is the enhanced PWM capable of commanding two 3-phase bridges (as advertised in the data-sheet)? Has anyone played with it? How soon an application…
Hi Eric Lee,
Good evening.
Kindly review the schematic of Buck converter using two LM5143 ICs.
Input:36V
Output:1.5V to 24V variable voltage with 30A.
We can obtain the variable voltage or not?
6232.Schmatic of LM5143.pdf
Thanks,
Jayaraman…
Other Parts Discussed in Thread: 66AK2E05 , TCI6638K2K Hi all,
I have 2 Blackhawk USB560-M emulator(one of this RevG, other not recognized). I have two board: one 66AK2E05 evm and one custom design board with TCI6628K2K SoC. So I checked if Blackhawk…
Hi All!
Most of our previous projects was for DSP C6416, and we were using Linear Assembly Optimizer a lot.
Now we are porting one existing project to C66 Keystone which is new for us. Checking output, produced with Linear Assembly Optimizer we…
Henry-liu,
What kind of support do you need? This is a very old IC and there are more current ICs that have better support for resonant topology.
I have included one of the design Seminars for the older ICs as an attachment to this response. Hopefully…
Hi Colin,
The problem is that the default flash parameter settings for the device are configured for a Li-Ion battery. There are many parameters that need to be updated for lead acid. I am attaching a spreadsheet that should be helpful to find the new…
HI,
Now I have a new problem. I want to run vision_app to use our sensor driver to confirm whether i2c2 can be used normally. While executing the script in vision_app, IPC failed to initialize. Because the design of the board currently used is different…