Part Number: BQ24765 When using the 24765 to control the charge of a LION battery, how would the host typically differentiate between a fully charged battery and a battery disconnect?
Part Number: BQ24765 Hi
How to improve the problem of RE radiation exceeding the standard in charging process ?
Below pictures show the test results.
1. When the adapter is inserted, BQ24765 starts to work.
2. When the adapter is not inserted, BQ24765 does…
bq24765 is not good for 1 Li-ion battery. The short protection is a 3.6V level and 2.5V level.
The bq24765 includes a foldback current limit when the battery voltage is low. If the battery voltage is less than 3.6 V but above 2.5 V, any charge current…
Part Number: BQ24765 Other Parts Discussed in Thread: BQ24171 , BQ24172 , BQ24780S Battery charger team - any issues with using the BQ24765 with a 5V input source and not the 'minimum 7V' source in the datasheet.
I see that the 5V source passes…
Part Number: BQ24765 I followed the link from the bq24765 page on TI.com and see a reference for this SMP-BQ24765-MVK eval board. The link clearly states that it is no longer offered but there is a request form for the board and schematic file. I have…
Part Number: BQ24765 I have a design using the bq24765 charge controller. My question is related to the use of the thermal pad. I used the recommended four layer board with a large number of small feedthroughs to all layers under the thermal pad. It works…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ40Z50 , BQSTUDIO , BQ24765 The technical reference has the following description, but sometimes there is no SMBus communication.
There is no access for only one cycle, and it will be restored from…
Hi Anthony, We've tried the BQ24160. Sadly it's suffering the same. When the battery is connected and a good voltage >3.9V I2C comms seem to be stable. Below 3.9V or when no battery is connected we get the SDA line being held by the BQ chip. We…
Other Parts Discussed in Thread: BQ24765 , BQ40Z50-R1 Under certain conditions the BQ24765 ACOK line is being pulsed low at approx. 5ms intervals.
This occurs when CE is high and the (BQ40Z50-R1) fuel gauge is not allowing current
from the BQ24765 to charge…
Other Parts Discussed in Thread: BQ24765 Hello guys,
My customer is evaluating BQ24765(SMBus-Controlled Multi-Chemistry Battery Charger With Integrated Power MOSFETs). They rarely found that SDA was fixed low when BQ24765 was controlled by MCU via SMBus and…