Part Number: BQ4802Y Tool/software: Hi team,
I am using BQ4802Y in my design. i had connected CEIN with VCC. Datasheet describe this pin as a chip enable input.
I have a doute that if it is a chip enable than it should be logic high in both mode (Powered…
Part Number: BQ4802Y Tool/software: Hi Team,
I am using BQ4802Y in my project. During testing i notice that when my device is ON RTC will work perfectly. but when i power off the device RTC will not work and when i again turn power ON RTC will start…
Part Number: BQ4802Y Tool/software: Hello,
I have made a circuit with the BQ4902Y. I can not use any other IC for several reasons I that would be off topic here.
My circuit as such works. Meaning I have several IC on the bus. But I can not get any readings…
Part Number: BQ4802Y Tool/software: I'm searching for an example code for the BQ4802Y RTC with any processor that demonstrates how to initiate if the IC is fresh. But I can't find any codes related to BQ4802Y. If you know how to find any example code…
Part Number: BQ4802Y Tool/software: Hello,
I am using the BQ4802Y and have the 32768KHz quarz hooked up with no capacitors. It seems to work fine although I have not yet tested in the long run.The quarz is specified with a load capacitance of 12.5pF…
Part Number: BQ4802Y Other Parts Discussed in Thread: BQ32000 , BQ32002 , BQ4802LY I have a circuit exactly based on the PDF Datasheet on Page 1 HERE
The issue is that when I set the time, for example if I set it at 12:00:00 it will never cycle, never count…
Part Number: BQ4802Y
Why the BQ4802Y Clock is not keep clocking when system power down ?
I have setted /STOP=1 in cotrol register E and use CR2302 Li Battery for Vbc. but the clock is not continue clock while system power down.
I've checked the BVF flag…
Part Number: BQ4802Y I've use BQ4802Y as system real time clock. VCC is 5VDC, VBC=3VDC Li Battery. I set the /STOP=1 in control register(E) and ABE=1 in Alarm enable register(C). I've checked that Control Register(E) content=06h, Flags Register(D) content…
Part Number: BQ4802Y Greetings
I need to implement a Real Time Clock in an Arduino UNO design and A Raspberry PI design.
Although the use is not the same in each, the general scenario is to just assign a Date / Time Stamp to a specific event.
The preferred…