Hi Chris,
Thanks again for sharing detailed logs.
It seems there is some dependency on the MAC state machine preventing link with 0x0 = 0x140 until the system is fully booted or some delay occurs.
Is it possible to emulate the manual write in SW, with…
Part Number: TDA4VP-Q1 Tool/software: Hello Experts
As part of regulatory requirements we need to save the data which is stored in internal SoC memory to a NVM, Do you have the data for the following scenario or what details you need from our side to…
Hello Kadir,
You can't load the M4F example from the debugger for this Reset Isolation example, Since the M4F PSC module is disabled with the debugIsolationEnable = 1 flag .
If you want to load an M4F example from the debugger, this debugIsolatio…
Part Number: TM4C123GH6PM
Tool/software:
Hi, We have recently met a Tiva TM4C123GH6PM SW reset issue described below
Procedure
1. Set pin#64 (PD3) Analog function (AIN4) with enabling internal Pull up.
2. Execute software System Reset Request by setting…
Hi,
For BQ25302, REGN cap and BTST cap should be the same values as recommended on the d/s (Figure 9-1. Typical Application Diagram).
The following actions may be helpful for EMI: 1)Add 1nF PMID, VBUS, BAT Recommend X7R 1nF (0402) which typically has…
Hi
1.The test SW is tested using a ground ring, which is consistent.
2.Your SW test also has -2.9V, and the SW in TPS56837 below does not exceed -1V, which obviously exceeds the requirement, doesn't it? Or does the current SW exceeding requirements not…
Hi Fergus,
I have attached screenshots from the scope. Channel 1 (yellow) is the output and channel 2 (blue) is SW.
Interested to see whether you can replicated it.
Thanks,
Gabriel
Part Number: TMS320F28027 Other Parts Discussed in Thread: MOTORWARE Tool/software: Hello, E:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\boostxldrv8305_revA\f28x\f2802xF\projects\ccs\proj_lab11a Angle compensation is shown in the…
Part Number: DRV3946-Q1 Tool/software: SW Set: UCLO_EN =1;RIPPLE_THRS = 0X0;SR = 0X4
The configuration about drive hold current of typically value is 0.6A, minimum is 0.53A
According to the SW set, the output Hi-Z limit value is 0.53*68% = 0.36A
Test result…
Hello, E:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\boostxldrv8305_revA\f28x\f2802xF\projects\ccs\proj_lab11a Angle compensation is shown in the figure,
That E: \ ti \ motorware \ motorware_1_01_00_18 \ sw \ solutions \ instaspin_foc…