Part Number: BUF602
Hello,
I am using the BUF602 in an ATE (Automated Test Equipment) application and I would like to clarify a question related to power supply conditions.
In my setup:
- The −VCC pin of the BUF602 is always connected to a…
Part Number: BUF602
Hi, I’m using the BUF602 in a high‑speed application and I would like to power it with asymmetric supply voltages.
The datasheet states that the device supports a total supply voltage up to 12.6 V. If I power the buffer with V…
Part Number: BUF602 Other Parts Discussed in Thread: LM27762 I am using the BUF602 in a design with +/-5v supply rails. My +5v is coming from an LT3045 and my -5v is coming from an LM27762. Both of these regulators are supplied by the same +5.5v supply…
Part Number: BUF602 Sir, Madam,
In a new design we want to use the BUF602 exactly like presented by figure 34 in the datasheet: "Self-Biased, Low Impedance Mid-Supply Voltage Reference".
Some facts:
Vsupply is 10V
Cload is 100nF typ. (@ mid…
Part Number: BUF602 Tool/software: Hi, I'm trying to locate the thermal resistance from Junction-to-Case for BUF602IDBVT which is a SOT-23 package. I see on the data sheet that it lists Theta JA (150 C/W) and a max operating ambient limit of 85C. Can…
Part Number: BUF602 Other Parts Discussed in Thread: TINA-TI , OPA695 Hello all,
I wish to build a unity gain sallen key LPF using the BUF602, in order to convert a 32MHz CMOS clock to a 32MHz sine wave.
Since the BUF602 don't actually has a non-inverting…
Part Number: BUF602 Other Parts Discussed in Thread: TPS65133 , FDC2214 , TINA-TI Dear TI experts,
I have two questions about powering the BUF602.
First question, can I power BUF602 with TPS65133?
The TPS65133 is a ±5V output dual-rail DC converter…
Hello Yash,
Your noise signals aren't selected. You will want to select the "Noise (V^2/Hz)" dialog box to be able to view this trace.
Best,
Hasan Babiker
Good question, not sure why I did not put that in the datasheet, normally would do that for an op amp,
Anyway, it does say it needs a 1.3V output headroom - but, if your are going to 0V input on single supply input, that input stage is saturated also…
Part Number: BUF602 Other Parts Discussed in Thread: TINA-TI , , THS3491
Hi guys, I am simulating the circuit below at Pspice-TI and Tina-TI. I've got the same results at both tools.
I receive 4 analog signals from 50ohms SMA cables with 10Vpp from…