Hi:
I am a Enrique´s colleague.
Our device is an endpoint device that makes CPSW work in dual mac mode and ony have one ethernet interface port.
Attached is the "ifconfig -a" command output.
Attached is also the device´s dts and we are using the…
Is this it?
/cfs-file/__key/communityserver-discussions-components-files/138/0081.TPS2034D_5F005F005F00_dflfs05_5F00_pwr_5F00_interface_5F00_Safety-Certification_5F00_CB_5F00_NEMKO_5F00_CB_5F00_UL_5F00_E_5F00_test_5F00_report.pdf
Part Number: DRV5023 Other Parts Discussed in Thread: DRV5055-Q1 Hi,
May I know any solution that can compare with A1333 as below?
Thanks
Regards,
Eric
A1333-Datasheet.pdf
Part Number: DP83630 Other Parts Discussed in Thread: DP83640 Hello,
I have two questions related to the DP83630.
1) Question one:
in RMII mode do RX_CLK and TX_CLK need to be connected to the MCU MAC?
in the DP83630 datasheet (Attached) section…
Hi Markku,
You can view the IEC Certifications here: BQ25120A The BQ25150 does not have the IEC certification but the BQ25155 does.
Best Regards,
Juan Ospina
Hi Rogelio,
thanks for the clarification about the supported commands. So, that seems to offer two options to go ahead:
1. Using the vendor specific commands to get WBS working also on CC2564C. In best case, we can keep our implementation compatible…
Jerry
I have attached a pdf below. Go to the section, " How to change Tetris and Core PLL speed " and check.
4401.MCSDK UG Chapter Exploring - Texas Instruments Wiki.pdf
Regards
Shankari G
Hi Bin Liu,
exp1: gpio@22 on i2c1 has a similar situation.
I have connected R485 to GND many times, but the interrupt count of "irq 376" in "cat /proc/interrupts" is still 0, and pca953x_irq_handler is not called.
dts code:
&main_i2c1 {
exp1…
directory_structure.txt Hi Surya,
1. There is no modification in file system. It is downloaded directly from the site mentioned in the pdf file and it is a first time compilation.
2. Please check the attached directory structure.
3. Commit ID of…