Part Number: AM62A7-Q1 Other Parts Discussed in Thread: SK-AM62A-LP , AM62A7 Tool/software: Dear Forum,
I have found a contradiction between AM62A data sheet:
According to section 7.10.2.2.1 Power-Up Sequencing in CPU datasheet, notes 10 and 11, …
Part Number: SK-AM62-LP Other Parts Discussed in Thread: AM62A7 Tool/software: Hello Team
I have one SK AM62LP evm board with ID ASSY PROC124E2A where I want to use one of the expansion pin as GPIO , where I can connect LED and test . Here I am trying…
Hi David,
Please see the document below, I see Signal level = 1.8V, CLK Freq up to 200MHz, Data rate is up to 400MB/s. (see page.12).
/cfs-file/__key/communityserver-discussions-components-files/138/Phison-eMMC-153-Ball-pSLC-SPEC_5F00_v1.4-_2800_1_2900_…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: DRA722 Tool/software: Linux First explain what I call the normal opening system. It’s about two seconds after the screen is darkened, I see the car image.
When I use the manual script method to…
Hi Barak,
Thanks for the response.
I followed the above step but again I am getting the same error:
# ./calibrator plt calibrate
[ 1316.327423] wl1271: ERROR command complete timeout [ 1318.944610] wl1271: ERROR command complete timeout [ 1321…
Part Number: AM5708 Other Parts Discussed in Thread: AM5728 Hi:
I have a custom AM5708 based board with SDK6.02 Linux RT.
The board has 3 ethernet interfaces:
- eth0: connected to GMAC
- eth1: connected to prueth pruss2_eth
- eth2: connected…
Hi,
In theory, you can use it.
The loss of the cable (based on the type of the cable) is very high at 2.4GHz. So, it would affect the range of communication.
The length of the cable depends upon it's loss and the link budget. Longer length means…
Hi kyuil,
In case of eMMC ,reset can be done in 3 ways:
CMD0
HW_Reset
Power cycle
CMD0:(S/W RESET)
Sending CMD 0 with specfic arguments will do software reset of the eMMC .
H/W reset:
The h/w reset can be done by sending the RST_n…
Dear Customer,
Sorry for the late response.
Few years ago, I personally mounted the UBIFS on K2H board by following the guide given here. Go to section "Using_UBIFS_file_system"
6320.MCSDK UG Chapter Exploring - Texas Instruments Wiki.pdf
And…