Hi Ferdinand,
The Mini BLE Broadcaster reference design is discontinued. For a small form factor reference design for the CC2541 you can look at: www.ti.com/.../CC2541-POSTAGE-STAMP-RD
Regards,
Fredrik
for mmc dev 0
=> mmc dev 0
switch to partitions #0, OK
mmc0(part 0) is current device
=> mmc info
Device: mmc@fa10000
Manufacturer ID: 70
OEM: 100
Name: IB291
Bus Speed: 200000000
Mode: HS200 (200MHz)
Rd Block Len: 512
MMC version 5.1
High…
Part Number: CC2541 Other Parts Discussed in Thread: CC2543 , CC2540 About the CC2541 DIE_ID
Hi All,
I'm studying CC2543 BLE broadcaster example code (swrc291), and want to port this example to CC2541.
DIE_ID define in miniBLE.h and the define address…
Hi Paul,
If you use the type C device attached you don't need to put the shunt in J4 or J5 as the type C device can present the Rd in the CC1 or CC2 .
So you have see the 5V when you attached the test device in the type C connector ,right ?
The idea…
Hello Mars,
Look at my reply in this post: e2e.ti.com/.../353925
1.
To use basic mode you will need to rewrite the application code. some work is required. The PER test is designed for use with auto mode with automatic acknowledge packets sent in return…
Part Number: CC2630 Other Parts Discussed in Thread: CC2650RC , REMOTI , TIMAC , CC2530ZLLRC-RD our customers want to use the zigbee remote control, the remote control is not required to access the network. There are a few questions now. 1. When the remote…
Other Parts Discussed in Thread: CC2543 Hi All,
I'm study in CC2543 BLE broadcaster example code (swrc291).
in example, use the CC2543 DIE_ID to be the device address, and my question is
" Does the DIE_ID unique for each CC2543?"
DIE_ID define…
Part Number: CC2541 Other Parts Discussed in Thread: CC2543 ,
Hi All,
I'm studying CC2543 BLE broadcaster example code (swrc291), and want to port this example to CC2541 .
there are 2 segments of code to set output power:
==== 1. in the function miniBlePhyInit…
Part Number: CC2531 Other Parts Discussed in Thread: Z-STACK-ARCHIVE , CC2530ZLLRC-RD , Z-STACK Hi YK Chen,
TI MAC CC2531 ZLL device is not receiving any broadcast packet sent by other CC2531 ZLL RC device.
We have set the logical channel to 11. Able to…