Other Parts Discussed in Thread: CC430F5123 , CC430F5125 , CC430F5143 , CC430F5145 , CC430F5147 , CC430F6147 , CC430F5137 The IAR 5.40 release notes show added support for the following CC430's
CC430F5123
CC430F5125
CC430F5143
CC430F5145
CC430F51…
Other Parts Discussed in Thread: CC430F5123 Hello,
I am new in this field. I am trying to run simple code in CCS5.1.0 which is given below.
#include "msp430x22x4.h"
volatile unsigned int i; // volatile to prevent optimization
void main(void…
Other Parts Discussed in Thread: MSP430G2231 , CC430F5123 I'm trying to build an assembler-only program in CCS v5.1 and I'm running into trouble with my definitions.
I want to create several constants which are located at specific, sequencial locations…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…