Part Number: CD4010B-Q1 Tool/software:
Hi Clemens
1.Your suggestion for using a discrete Low Vgs threshold MOSFET for Hi to Low translation was welcome.
Perhaps the one issue could be that if Vil is Low Voltage on the 15 V side; the Vil for the…
Part Number: CD4010B-Q1 Tool/software: I would like to have some help with the Failure Mode Distribution for the CD4010B-Q1, this is usually included in the Functional Safety FIT Rate, FMD and Pin FMA report, but I cannot locate it in the technical documentation…
Part Number: CD4010B-Q1 Other Parts Discussed in Thread: CD40109B-Q1 , Hello,
I was previously using PN# CD40109BQNSRQ1 to level shift from 12v to 3.3v. I needed extra inputs so changed to PN#CD4010BQDRQ1. I am currently running vehicle turn signals…
Part Number: CD4010B-Q1 Other Parts Discussed in Thread: TXU0104 , SN74LXC8T245 I would like to use CD4010B-Q1 to translate digital lines from a 3,3V sensor to 5V uC
in The datasheet in the table "STATIC ELECTRICAL CHARACTERISTICS" there are VOL Max…
Part Number: CD4010B-Q1 Other Parts Discussed in Thread: SN74HC595 Hello,
Could you provide 3D Step file of CD4010BQDRQ1?
I cannot find 16pin SOIC package 3D step file in Ti website.
Regards,
Nicky
Part Number: CD4010B-Q1 Other Parts Discussed in Thread: CD4010B Hi team,
My customer is using the CD4010B chip now. The VCC voltage is 5v. When we remove the D147 , and not use the 12v_ON1 supply, the VDD voltage is 4.35v. Could you help me check why…
Other Parts Discussed in Thread: CD4010B-MIL , CD4010B-Q1 Hello,
We need a small variety of logic functions that will operate in an -10 to +135 C environment.
Since there does not seem to be anything meeting this rating, I thought of using parts similar…
Moataz,
As it looks on the data sheet, the CD4010B-Q1 only has test data up to 4 MHz. It may be possible to run it at higher frequencies, but we do not have data on that operation. Also, the specified transition times are 100 ns to 200 ns for 15 V to…
Part Number: AM26C31 Other Parts Discussed in Thread: ESDS314 , AM26LV31 , AM26C32 , AM26LV31E , TXU0104 , TXU0102 , TXU0101 , TXU0304 , CD4010B , TXH0137D-Q1 Hello Community,
We are selecting ESD & EOS protection for our RS4xx use case. We anticipate…