Other Parts Discussed in Thread: CD74HC4053 Please let me know about On resistance (Ron) of CD74HC4053.
・Min_value of Ron
・Temperature characteristics of Ron
(Customer want to know 0~45℃)
Best regards,
Satoshi
Part Number: TMUX4053 Other Parts Discussed in Thread: CD74HC4053 Tool/software: Hi All,
I have a question about the TMUX4053.
Is it not possible to use it with a power supply voltage of ±3V?
In 6.4 Recommended Operating Conditions, it looks like…
Part Number: CD4053B Other Parts Discussed in Thread: SN74LV4053A , CD74HC4053 Tool/software: Hi expert,
Do we have P2P devices with similar prices can replace CD4053BM96? Please also help to recommend similar prices devices if P2P devices are too expensive…
Part Number: TMUX4053 Other Parts Discussed in Thread: CD74HC4053 Tool/software: The recommended operating conditions Min for VDD is 5V. I will be operating with VDD=5Vtyp and VSS=-5Vtyp, and there is a possibility that VDD will be less than 5V.
Is…
Hello Simon,
The CD74HC4053 is a 3-channel 2:1 so I don't think you need to cascade. You can combine a couple of the channels as below:
Here is the propagation delay information for the CD74HC4053, is it fast enough?
Thanks,
Nir
Part Number: SN74AUC2G53 Other Parts Discussed in Thread: TMUX1133 , CD74HC4053 , Tool/software: I need to switch between 2 different negative voltages to the common output.
The negative voltages range between 0V and -1V
1) Can I connect the Vcc…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TMUX4157N , CD74HC4053 , TS5A3159-EP Tool/software: We are interested in the SN74LVC1G3157DBVR and need it to operate at -55°C. Do you carry a version of this part that meets this requirement
Part Number: SN74LV4053A Other Parts Discussed in Thread: TMUX4053 , TMUX1133 , CD74HC4053 , Hello guys,
One of my customers is using SN74LV4053A for their mas-production products.
The are looking for new TI alternate device for SN74LV4053A because…
Part Number: TS5A22362 Other Parts Discussed in Thread: TPS60403 , CD74HC4053 Dear expert,
Input signal is +/-2.5V when in 3.3VCC application.
Based on recommendation operating condition, TS5A22362 cannot support this application. (3.3-5.5=-2.2V…
Part Number: CD4053B Other Parts Discussed in Thread: CD74HC4053 I'm looking for a faster version of the CD4053 (Analog SPDT Switch).. I wish it could switch the signal in about 5 nS.
Is there a component with these characteristics?