Part Number: CDC3RL02 Hi Team,
Does the following table show the total power consumption of the device? How to calculate the total power consumption of the device accurately?
Part Number: CDC3RL02 Other Parts Discussed in Thread: LMH2191TMEVAL , Hello,
I noticed there is no EVM for this part. Is there an EVM for another part in this same family of parts that would have the same characteristics?
Thanks,
Daniel Ri…
Part Number: CDC3RL02 Other Parts Discussed in Thread: LMH2191TMEVAL , LMH2191 Hi team,
Customer wants to use two clock buffer cdc3rl02 cascades to output three channel clock signals, but has concern that the voltage range may not enough, there are…
Part Number: CDC3RL02 Other Parts Discussed in Thread: LMK1C1102 Team:
Can i use this device for 32.768KHZ input? I notice that it is just for 10MHZ and above. If not ,could you recommend one which is used for 32.768KHZ?
Part Number: CDC3RL02 Hello team
Could you let me get your advice on the below query?
VBAT : 3.3V / 3.6V / 4.2V
Requirements
Current Consumption Data
Condition
VBAT : 3.3V / 3.6V / 4.2V
Cap Load : 10pF
26MHz…
Part Number: CDC3RL02 Team
One thing, I would like to share is below.
Currently I am under competition with competitor Part from ONSEMI.
And my customer has informed that the part has total 4mA current consumption with 52MHz output x 2channel. …
Part Number: CDC3RL02 Hi All,
CDC3RL02 has two parts.
CDC3RL02 B YFPR and CDC3RL02YFPR.
This is a difference by backside coating.
Does the presence or absence of backside coating affect performance (reliability test, etc.) ?
Best Regards…
Part Number: CDC3RL02 Hi team,
I have a question regarding CDC3RL02. Here is my basic setup:
VBATT = 3.3V
MCLK = 24MHZ 1.8V CMOS
LDO = unused/floating
With the above, my output looks like Image 1 (below). However, when I drop VBATT to 1…
Part Number: CDC3RL02 We're using the device to allow us to choose between two clock sources (i.e 2 instances of the CDC3RL02). This means that two CLK_OUT pins are tied together.
Connected in this way, is there any risk of back feeding:
Causing…