Hi Allen,
1. LMK00334 does have normal HCSL output. CDCDB800/CDCDB400 do have LP-HCSL outputs.
2. The resistors should be placed at the outputs of the LMK00334.
3. AC coupling is optional, or depends on the input signal. Most input signal standards can…
Hi Jacob,
CDCDB2000 does not support a 100 ohm impedance (per datasheet spec) because of the 85 ohm integrated termination.
I suggest using 3 CDCDB800 / CDCDB803 devices instead. These devices can be configured for 100 ohm impedance.
Regards,
Jennife…
Hi Danny,
We will offer a new device CDCDB800 that is a better fit to replace the competitor device. Please send us an email at cts_buffer_flex@list.ti.com and we can provide you some more information on this product.
Kind regards, Lane