Part Number: CDCE62002
Hi team,
I have a question regarding the Internal Loop Filter configuration of the CDCE62002.
When using the PLL Loop Filter Tool and selecting the Internal Loop Filter option, the tool generates a warning indicating that…
Part Number: CDCE62002 Other Parts Discussed in Thread: CDCM6208 , LMK03328 , CDCM6208V1 , CLOCKPRO Hi team,
My customer is evaluating potential replacement devices for CDCE62002 and would appreciate your guidance on suitable alternatives within the…
Part Number: CDCE62002
Hello,
We are using CDCE62002 as a jitter cleaner and investigating a PLL lock-time related issue.
According to the datasheet, the VCO operating range is specified as 1.750 GHz to 2.356 GHz.
I would like to ask whether operating…
Part Number: CDCE62002 I would like to know the maximum operating temperature range. In the datasheet I have found the junction temperature (125°C) and the recommended temperature range (up to 85°C). 40 degrees of difference between these two values seems…
Part Number: CDCE62002 Other Parts Discussed in Thread: CLOCKPRO Hi All,
I have a configuration question regarding the CDCE62002. The customer is using the device in jitter cleaner mode and would like to keep the output frequency at 297MHz. When evaluating…
Part Number: CDCE62002 Hi,
I am currently experiencing an issue with the clock cleaner CDCE62002. I use the clock cleaner to convert frequencies from 74.25 MHz to 74.25MHz or 148.5 MHz to 148.5 MHz. I need a perfect x1 conversion. Most of the time,…
Part Number: CDCE62002 Hi,
We are using CDCE62002 for Jitter cleaning.
The device seems to have temperature Characteristics for lock time.
Because,
1. We input signal when the package is about 100℃, then CDCE62002 does not lock.
2. As the package…
Part Number: CDCE62002 Tool/software: Hi,
Good day.
We are thrid part for programming, and we are developping the algo and tool for customer programming.
Could you help to provide the configuration/programming file of CDCE62002RHBR for programming…
Part Number: CDCE62002 Hi,
we are using cdce62002, for converting ref clock of 13MHz to a clock of 204.8MHz.
below is the configuration we are using.
the issue is that we are facing many spurs at the output (please see attached screenshot of spectrum…
Part Number: CDCE62002 Hello expert,
Do we have timing requirement between PD and VCC? I checked datasheet page 10 and there is #PD reqiurements but i didn't find the graph to specific point out the relation between VCC and #PD. Could you provide the…