You can bypass on-board crystal and use an external reference at a desired frequency. What are the output frequencies you desire? Do you have any external reference that you can provide? Or you can swap out the on-board 30.72MHz crystal to another crystal…
Other Parts Discussed in Thread: CDCE62002EVM , CDCE62002 Hi ALL
I need to generate a 20 MHz clock through CDCE62002EVM. I downloaded the GUI Software.
I selected AUX as source. I used frequency planner to set the dividers for output of 20 Mhz. I…
Other Parts Discussed in Thread: CDCE62002EVM , CDCE62002 Hi all,
I am having problems using the CDCE62002EVM. I would like to set up the EVM and then program the CDCE62002 part number that I implemented in a project. I tried the GUI in two different…
Jack,
The GUI for CDCE62002 is located here: https://dr-download.ti.com/software-development/gui-for-evaluation-module-evm/MD-kLq1ch5kGS/01.00.00.0C/scac112c.zip
Per Cris' earlier statement, this is on the product page:
TCB files are for usage…
Part Number: ADS42LB49EVM Other Parts Discussed in Thread: CDCE62002EVM , Hello,
I'd like to ask about the max voltage allowed on the clock input of the eval board.
I have CDCE62002EVM and it seems in lvcoms mode its output is 3.3 volts, which I…
Hi Sugawara-san,
TISC Pro does not support CDCE62002 and the CDCE62002EVM does not require USB2ANY, it can be directly connected to a PC.
The GUI for the EVM is available here: www.ti.com/.../scac112
Hi,
Thanks for the reply,
Please look below document,
http://www.ti.com/lit/ug/scau034/scau034.pdf
Two/Four Output Low Phase Noise Clock Evaluation Board - Page - 3
The second input (AUX IN) can support a crystal in the frequency range of 2MHz…
Part Number: CDCE62002 Hello to whom it may concern,
I have two question about CDCE62002.
Q1 ; The VBB is connected 1uF capacitor in the datasheet.
However, It is connected 10uF at CDCE62002EVM.
Which one is correct?
Q2 ; About output…