Part Number: CDCE62005 Hello,
Our customer used two CDCE62005 for cascade application. But some of the board the second CDCE62005 couldn't be lock.
His description is as following:
Our circuit is fully referenced to TI's official 6678 development…
Part Number: CDCE62005 Hello,
The customer attempted to create the configuration below using the CDCE62005 GUI, but an error occurred.
- AUX IN : 25MHz
- Output 0 : 100MHz / Output 2 : 66.667MHz / Output 3 : 100MHz
Below is the error message…
Part Number: CDCE62005 Dear TI team,
I have A situation where I am outputting an LVDS Clock output from CDCE62005 to LTC2107IUK @ 200MHz.
But the LVDS lines are crossing each other on the PCB. I do not want much layer changes as I need a dual pair…
Part Number: CDCE62005 Dear TI support,
Appreciate your answers to the following questions below:
1. Does CDCE62005 come pre-burned from TI with our specific specifications?
2. The clock generator need to be configured every power-up?
3. Is there…
Part Number: CDCE62005 Other Parts Discussed in Thread: DAC3171 , LMK01801 Hi Team!
My customer is interested in using DAC3171 to convert digitized ultrasound data to an analog output.
They want to use a 400MHz LVDS clock from FPGA to drive the DACCLK…
Part Number: CDCE62005 Other Parts Discussed in Thread: TMS320C6655 Hello,
I connect CDCE62005 to TI DSP TMS320C6655, but I using only 3 input clocks in this DSP, (Core, SGMII, and DDR) so I need only 3 LVDS outputs from CDCE62005.
Should I leave…
Part Number: DAC3482EVM Other Parts Discussed in Thread: CDCE62005 Hi
I have DAC3482EVM. I'm trying to configure the CDCE62005 integrated on the board. Although I do the same configuration, I see my clock signal, which should normally be set to 64Mhz…
Part Number: CDCE62005 Hi
We have tried loading registers in CDCE62005 using Control software. The problem is we couldn't write in EEPROM. We have to load the register settings every time we power up.
What could be the possible reason for EEPROM write…
Part Number: CDCE62005 hello, I want to initialize and program CDCE62005 with my own circuit. But now I have some problems.
First, I am not sure whether the peripheral circuit of the chip built is correct, I cannot confirm whether the chip works, and…
Part Number: CDCE62005 Hi,
We are using CDCE62005 Clock generator Ic to clock the DSP Processor TMS320C6678ACYPA.
We are planning to program IC through SPI.
Can we have any suggestion for programming?
If we use Header to program SPI, which emulator…