Part Number: CDCE906 Other Parts Discussed in Thread: CDCE913 Tool/software:
Hi,
Can you advise me to resolve my t\problem when I used Clock Pro.
I have downloaded Clock Pro V1.2.1 and tried to configure CDCE906.
However, I can’t find CDCDE906…
Part Number: CDCE906 Other Parts Discussed in Thread: CDCE913 , Tool/software: Hi,
Please advise on on my question bellow.
The CDCE913/925 datasheet insist as follow.
9.3 Power Supply Recommendations
When using an external reference clock, XIN…
Part Number: CDCE906
Tool/software:
Hi, I am trying to create a config file for the CDCE906 chip using TI Pro Clock's Programming Assistant. I need to set specific values for the divider and multiplier, but it only allows me to set the input and output…
Part Number: CDCE906 Tool/software: Hello E2E Experts,
Good day.
I got some quetions about cdce906.I configured the registers, with an input clock of 8 MHz. The output of Y0 and Y1 is 8 MHz, and the output of Y2 to Y5 is 64 kHz. I wrote this into…
Part Number: CDCE906-706PROGEVM Other Parts Discussed in Thread: CDCE706 , CLOCKPRO , CDCE906 , CDCEL9XXPROGEVM , Tool/software: I was trying to program CDCE 906 chip with CDCE 906/CDCE706 Programming EVM (Rev B). I downloaded the CLockPro Software but…
Part Number: CDCE906-706PERFEVM Other Parts Discussed in Thread: CLOCKPRO , CDCE906 Hello,
2 years ago this questions has been already asked, but it was not really answered: Although the readme states, that ClockPro supports CDCE906, it is not listed…
Part Number: CDCE906 Other Parts Discussed in Thread: CDCE913 , CLOCKPRO Hi,
Do we have any demo code or example code we can share for setting up the CDCE906? I want to configure its clock output via the I2C bus ,but I only have the chip connected to…
Part Number: CDCE906 Other Parts Discussed in Thread: CDCE925 Hi,
I'm looking for a clockgenerator at 3.3V with the following:
Clock input: CMOS 25MHz, external oscillator
Outputs at 3.3V levels
Output1: 48.000MHz
Output2: 13.271MHz
Output3…
Part Number: CDCE906 Other Parts Discussed in Thread: TIDA-00080 Hello.
I have investigated the CDCE906 on TIDA-00080.
After I successfully re-programmed the data on CDCE906, I turned off the power and turned on again.
Then I realized that CDCE906…