Part Number: CDCE913 Hello Team,
I got a question from my customer.
The customer tried to load setup file.
However, Clock Pro generated error massage.
The customer operated as below sequence.
1, run Clock pro and set up frequency (fin: 18.432MHz, fout…
Part Number: CDCE913-Q1 Please check on correctness of below datasheet statements at page 23:
0≤R≤511 instead of 0≤R≤51 & unit µs seem to be wrong
P=4-int(log2 (N/M)) instead of P = 4-int(log2 N/M)
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCEL9XXPROGEVM Hi TI-team
I use CDCEL9XXPROGEVM.
But The PC( windows 10) does not recognize EVM.
https://e2e.ti.com/support/clock-and-timing/f/48/p/960089/3549356?tisearch=e2e-sitesearch&keymatch…
Part Number: CDCE913 Other Parts Discussed in Thread: CLOCKPRO
Hello
Would you please let me know the way how to change the fout on the fly without lost of fout / or unexpected frequency of fout?
Q1
How can I change fout(MHz) on the fly by changing N…
Part Number: CDCE913-Q1 Hello Team,
I got some questions from customer about the CDCE913-Q1.
Q. How much propagation delay from VDD(1.8V) ramp up to start output clock?
Q. How much propagation delay from VDD(1.8V) ramp down to stop output clock?
[Condition…
Part Number: CDCE913 Hi,
My customer would like to expect a data retention period themselves.
How much is the activation energy?
Which is the nearest from the followings?
(a) X < 0.6eV
(b) 0.6eV < X < 1eV
(c) 1eV < X
Best Regards,
Kuramoch…
Part Number: CDCE913 Hi,
My customer is evaluating the CDCE913 and inquiring as below;
Could you provide the term of keeping data when writing 100 times at except for 85℃?
Best Regards, Kuramochi
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE925 , CDCEL913 , CDCEL925 Hi all,
We are using Zynq-7000 in our custom board and Linux version 4.14.0.
We are using CDCE913 clock synthesizer in our custom board and have to configure for 100Mhz.
…
Part Number: CDCE913 Hello Noel,
One of a customer worry about CDCE913 stop production. will it happen? May I also ask whether there is a next generation of CDCE913, do you mind send me the updated roadmap of clock products by email?
Many thanks!
Part Number: CDCE913 Hi,
I inquired about the data retention period on the previous thread.
My customer requests the data retention period data at room temperature.
They use it to consider the effect of temperature on the retention period.
Best Regards…