Adarsh,
I would recommend for the CDCE913 either using a separate ferrite bead for VDDOUT or using the same ferrite bead for all VDD & VDDOUT, rather than keeping VDDOUT straight from the supply. I have re-assigned this to the proper team for the SN65DSI83…
Part Number: CDCE913 Hello,
According to following E2E thread, even though SCL and SDA are 3.3V tolerant, it is not recommended to drive the input when VDD = 0V.
https://e2e.ti.com/support/clock-and-timing/f/48/p/769394/2845927?tisearch=e2e-sitesearch&keymatch…
Part Number: CDCE913 Other Parts Discussed in Thread: LMX2594 , CDCE62002 Dear Sir,
My customer is interesting in using CDCE913 for reference clock generator.
I could not find simulator nor a phase noise performance data/graph in the datasheet.
Do you…
Part Number: CDCE913 Hi,
I'm facing an issue of I2C byte access.
Upper figure shows byte-write access to 0x2. I can see ack. Then bottom figure shows access to 0x1, and nack is issued. Is my operation wrong?
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE62002 Is there any similar one to compete with NB3N5573? Please advice. thanks.
Regards
Brian
Part Number: CDCE913 We are using the CDCE913 to generate a 27MHz output from a 10MHz input. The 10MHz comes from a GPS receiver and what we are finding is that if the 10MHz is not connected when the unit powers up and the 10MHz is connected afterwards…
Part Number: CDCE913 Hi Team,
I believe SSC function is supported to all VCO frequency range which is from 80MHz to 230MHz, am I understanding correctly ?
If there is any limitation, please let us know.
Thanks and Best Regards,
Kawai
Part Number: CDCE913 Other Parts Discussed in Thread: LMK05028 , LMK05318 , LMK04821 Hi,
I need a clock generator, Input: a square wave with a 50% duty cycle of 100k frequency;
Output: a square wave with a 50% duty cycle of 200k frequency…
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE706
Hi Team,
Please allow us to ask you about the CDCE913 SSC modulation frequency.
CDCE706 has a SSC modulation frequency selection function, however, CDCE913 does not. Based on the "SSC Modulation…