Part Number: TIDA-010057 Other Parts Discussed in Thread: CDCE949 , CDCEL9XXPROGEVM , CLOCKPRO I am building a copy of the TIDA-010057 board since it is not for sale. The design guide (TIDUEP0–May 2020) states at page 20 that the config file of the CDCE949…
Part Number: CDCE949 Other Parts Discussed in Thread: CLOCKPRO Hi Sir
May we must connect to EVM when we use TI Clock pro?
Because we have no EVM on hand.
may you pls help use TI Clock pro set CDCE949 Y2 output 66MHz,then output TXTfile to us for…
Part Number: CDCE949 I am looking for explanation of the P Q R parameters for CDCE949. I can choose N & M parameters and I can calculate the P Q R parameters. Though not specifically stated, it seems that results with R = 0 may be be desired above R …
Part Number: CDCE949-Q1 Hi team,
1) Why the EVM has AC coupling(C4) at the clock input even though it's LVCMOS input?
2) For Xin/CLK-pin on the IBIS model, which XTAL input or LVCMOS input is modeled? My customer want to simulate with LVCMOS input…
Part Number: CDCE949-Q1 Hi team,
Can we provide the evaluation result(min/max or ave+stdve) for leakage current on Yx-pin in 3-State output?
Best Regards,
Part Number: CDCE949-Q1 Other Parts Discussed in Thread: CDCE949 Hi Expert,
The crystal vendor said that the crystal stability is -90ppm, what's CDCE949 recommend? Or how to decide it? Thanks!
Part Number: CDCE949-Q1 I would like to create various clocks by clock generator. I guess this device CDCE949-Q1 is close to the correct as far as I searched.
I would like the solution which can handle various clocks of voltage (1.0Vpp, 1.8Vpp and 3…
Part Number: CDCE949 Hello,
I would like to create 25 MHz PLL out and I have found two PLL settings:
- Input clock is 27 MHz.
- Y7 is my target PLL in the attache TI Clock Pro capture file.
1. first settings (2015_1223)
M = 486
N = 3600…
Part Number: CDCE949-Q1 Hi team,
Could you check the start up time from VDD ramp(S0 pulled up to VDD) to Yx output?
And, could you check the required wait time from VDD ramp to ready I2C access.
Best Regards,