Part Number: CDCI6214 Hi Team,
This is technical support request for CDCI624. When CDCI6214 PLL unlock occurs, except for powering off and restarting, no matter how you configure the chip or RESET, it cannot return to normal. After merging the i2c of the…
Part Number: CDCI6214 Other Parts Discussed in Thread: CDCE6214 Hi,
I wish to generate 2MHz clocks from channel 2 and 3. But the measured output clocks are always 760KHz. The input is 80MHz LVDS ac-coupled input.
Below figure is block diagram in TISC…
Part Number: CDCI6214 Other Parts Discussed in Thread: CDCE6214 , LMK3H0102 I want to know how much current can the LVCMOS and LVDS channel outputs can source or sink to an external devices. I couldn't find any parameter for this in the datasheet
Part Number: CDCI6214 What is the limitation for generating <44.1kHz on the outputs?
I'd like to use this to generate lower frequency phase synchronized outputs.
Part Number: CDCI6214 Hi team,
Support need.
When CDCI6214 is in MODE1 mode, GPIO1~GPIO4 are multiplexed as 4 CHANNEL output OE pins. The manual describes that the falling edge/rising edge of OE1/OE2 corresponds to the clock output of the EN/DISEN…
Part Number: CDCI6214 Hello,
About CDCI6214 TICSpro, we could find that there is a note about pll_ndiv. It means: Ncount value. The actual value will be 4 less than programmed value. Also - during the calibration - the value will 4 times (minus 4) the programmed…
Part Number: CDCI6214 Dear Team,
We connected the left Crystal in the figure below to XIN and Xout of 6214, and configured 22PF capacitors on the two pins of the crystal. Now we find that the crystal on some single boards cannot start to vibrate. Our…
Part Number: CDCI6214 Other Parts Discussed in Thread: , USB2ANY Hi,
1. Use TICS PRO GUI to control CDCI6214EVM, can't read and write registers, according to the description of User's Guide, there is no EVM Default in the Default configuration dropdown…
Part Number: CDCI6214 Dear Team,
May I know could our GUI generate a tcb file?
The customer's factory can only use the tcb file to programming the IC.
Many Thanks,
Jimmy