Part Number: CDCI6214 Hi there,
customer requirement:
input 52Mhz LVDS CLK, output 26Mhz LVDS CLK, is it achievable by CDCI6214?
if yes, what's the expected jitter caused by CDCI6214?
BRs, Shubiao
Part Number: CDCI6214EVM Where can I find any information on how to use the Wizard to set target frequencies? There are are two many options in the Wizard
Part Number: CDCI6214 Hello,
My customer would like to output the same polarity LVCMOS signals at Y2P and Y2N. What values should be set for ch2_cmos_pol and ch2_outbuf_ctrl respectively? Best regards, K.Hirano
Part Number: CDCI6214 Other Parts Discussed in Thread: CDCDB800 Hello Expert,
Our customer want to know which register they have to set for 100khz output.
Could you please give me example setting for this?
Their target output is 100khz.
Best regards…
Part Number: CDCI6214 I have a technical support question regarding your CDCI6214 chip. we are using this clock generator to redistribute a single ended 125MHz clock from a phy. We are using the REFP input for the 125MHz signal, as per the datasheet,…
Part Number: CDCI6214 Hi Team,
According to the datasheet, I didn't found the requirements of VXIN when crystal mode. Is there any VXIN range?
Also please provide a XIN pin's requirements of the voltage of Vhigh, Vlow, Vpp.
Great thanks
BR…
Part Number: CDCI6214
Hello,
There are 55 registers described in the datasheet SNAS734E Table 15. However, Ticspro generates 70 register values. What are the descriptions of the non-described registers?
Kind regards,
Irmak
Part Number: CDCI6214 Hello, My customer has a couple of questions as follows. Q1: When gpio0_input_sel = 0, without power cycle, REFSEL and EEPROMSEL can be resampled by toggling RESETN/SYNC (High to Low to High)? Q2: Without RESETN/SYNC toggling, is…
Part Number: CDCI6214 Hello,
In our application. The ch1 is 50M AC-LVPECL, ch2 is 100M HCSL and ch3 is dual 25M LVCMOS. Input is 25M OSC.
For 50M AC-LVPECL. The chipset input criterion is <1ps@12k~20M, But our measure result around 1.5ps.
Can we…
Part Number: CDCI6214 Hello. I need to run the CDCI6214 as zerodely buffer. The input is 100MHz, differential HCSL type connected to REF input. The outpus shall be as following - Y1, 100MHz HCSL type - Y4, 100MHz HCSL type The I2C interface of CDCI is…