Part Number: CDCLVC1102 Hi
We are designing a PTS(Product testing System) where some High frequency 208MHz clock is used in DUT device and here we have to check its frequency through some POGO pins, then came to our board then go through cable connector…
Part Number: CDCLVC1102 Hi Sirs,
Sorry to bother you.
As title, could you help check our schematic?
The VDD will used +3.3V and to reserved LDO +2.5V,
Because we didn't find Pin 1G Output enable input voltage range from datasheet,is ok for our…
Hi Howard,
The minimum input slew rate for the CDCLVC1102 is 1 V/ns. It can support 0.8-0.9V/ns input slew rate, but this operating point is outside of the recommended operating conditions, therefore you might get performance that exceeds the electrical…
Part Number: CDCLVC1102 Hi team,
I'm looking to cross IDT's 83026BGI-01LFT because I don't like the non hot swappable characteristics of that device. I believe CDCLVC1102 is TI's best replacement. What are the hot swappable characteristics of the CDCLVC1102…
Part Number: CDCLVC1102 Other Parts Discussed in Thread: LMX2581E , LMK04826 , SN65MLVD200A , Hi,
I Plan to use external 10MHz reference clock which produces differential signal (voltage out is 0.84Vlow - 1.6Vhigh). I want to distribute this signal…
Hello Kay CDCLVC1102 is a plain buffer. We dont have exactly the same part. What is the input/output frequencies and what is the jitter spec? We might find an alternate part based on that. Best regards Puneet
Other Parts Discussed in Thread: CDCLVC1102 Hi,
I would like to use CDCLVC1102 as 135MHz clock buffer. I only need one clock output (Y0).
To prevent its other clock output (Y1) from noising the board, I want to put parallel capacitor from Y1 to GND…
Part Number: CDCLVC1102 Hello,
Can you please provide the Junction-to-Board Thermal Resistance (Theta-JB) for the device CDCLVC1102PW ??
Regards,
Goutham Sharma
Part Number: CDCLVC1102 Hi,
I've noticed that the datasheet for the CDCLVC11xx family specifies an output current of 50mA. Is this value per output, or the combined maximum? By the logic of it, it seems to be per output, but I want to be sure.
Kind…
Other Parts Discussed in Thread: CDCLVC1102 Hi, I was planning to use the cdclvc1102 to buffer a 3.3V CMOS square wave input(10MHz output freq) from a clk generator chip to generate a clean 10MHz sine wave by passing the square wave through a good band…