Part Number: CDCLVC1106 Other Parts Discussed in Thread: LMK00804B , CDCLVC1104EVM , LMK00804B-Q1 Hello,
I wanted the input pins details of CDCLVC1106, is there Pull up or Pull down and Impedence.
Can I use LMK00804B outputs as inputs to CDCLVC1106 (LVCMOS…
Part Number: CDCLVC1106 Other Parts Discussed in Thread: CDCLVC1102 , LMK1C1104 Hi Team, we would like to confirm the load capacitance for CDCLVC1106 and CDCLVC1102.
Thank you very much.
Regards,
Mark
Part Number: CDCLVC1106 Hi,
Customer would like to use our clock buffer for Intel ethernet chip I210, and Intel reference circuit has two cap C1/C2, is that ok to put these cap at our buffer output? Will it impact our buffer performance?
Regards,
L…
Part Number: CDCLVC1106 Hi.
I am using a CDCLVC1106 in an application where I need to distribute a precision 10MHz square wave clock to several pieces of lab equipment. On most of the equipment the receive side is 50-ohm terminated (as is good transmission…
Part Number: CDCLVC1106 Dear Technical Support Team,
Could you please share the input capacitance of CLKIN?
I'd like to check that the load capacitance of oscillator can withstand the input capacitance of CLKIN.
Best Regards,
ttd
Part Number: CDCLVC1106 Other Parts Discussed in Thread: SN65LVDT14 Hello Team,
Can you help with the question below:
Need clarification on CDCLVC1106 clock buffer’s datasheet slew rate specification. We’re planning to use this part downstream…
Part Number: CDCLVC1106 The distance between the output of CDCLVC1106 and the load is about 5 cm, which transmits 38M clock signal. Does it affect the integrity of the signal? Will it affect the rising and falling edges of clock signals? What is the maximum…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: CDCLVC1106 , , CDCLVC1104 Hi Team,
Greetings !
I have some queries regarding the Fbead current and impedance ratings which are used to filter the power supply for buffer ICs CDCLVC1310, CDCLVC1104…