Part Number: CDCLVC1310 Other Parts Discussed in Thread: AM6421 , Hello, We are using CDCLVC1310 clock buffer in one of our designs which is based on AM6421 processor. While refering to EVM schematic "PROC101C(004)_SCH", we found some hardware circuit…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: CDCM1802 ,
Tool/software:
Hello - the datasheet for the CDCLVC1310 device specifies ouput duty cycle to be 45%/55% (5% distortion) with an input frequency of 125MHz and 50%/50% input duty cycle…
Part Number: CDCLVC1310 Hi,
Customer request the DPA report for CDCLVC1310RHBR and CDCV304PWR, the reprot include t est items, test methods, test results, conclusions and so on,
We can't search in the TI website, please kindly support, thanks.
Part Number: CDCLVC1310 Other Parts Discussed in Thread: TMDS64EVM
Hi ,
I’m driving a 25 MHz LVCMOS clock from an Abracon ASDMB‑25.000MHZ‑LY‑T MEMS oscillator into a single‑ended buffer . I consistently see no clock when probing directly at the oscillator…
Part Number: CDCLVC1310 Hi TI Teams,
Can u help to check the schematic of CDCLVC1310? The schematic is as below.
CDCLVC1310RHBR SCH.pdf
Thanks,
Kind Regards
Part Number: CDCLVC1310 Hello
1、schematic check
We use CDCLVC1310 as CLK BUFFER,The clock input and output circuits are shown in the following figure,please help check if the circuit is correct.
The detailed information of the circuit is as follows…
Part Number: CDCLVC1310 Hi Expert,
my customer is using CDCLVC1310 in server mother board, as single-end LVCMOS 50MHz input and output for FPGA system reference clock, but we don't find the input slew rate in datasheet, could you help to check it? thanks…
Part Number: CDCLVC1310 Dear team,
I cannot find the ESD rating data from device datasheet.
Could you share ESD information with us?
According to datasheet description, "these devices have limited built-in ESD protection"
Does that mean we…
Part Number: CDCLVC1310-EVM I am using the CDCLVC1310-EVM. I am supplying 3.3V to both VDD and VDDO. I'm using the onboard 25MHz crystal oscillator to measure a square waveform, but am just getting a saw function instead. The output also varies from …
Part Number: CDCLVC1310 Hi team,
For the CDCLVC1310 datasheet, it says input duty cycle is 40%-60%. Currently my customer's duty cycle is 1hz(11%), whether it has risks? Thanks.