Q1. Will there be some voltage levels on the output pins of CDCLVC1310 IC because of the other ICs are fanned-In ? If some volatage level is there, then what could be the possible value?
A1. When CDCLVC1310 is powered down the outputs are not driven…
Part Number: CDCLVC1310 Hi Team,
What's the TI recommend termination for the unused output pins? Floating or connect to GND with 50ohm resistor?
Thank you.
Part Number: CDCLVC1310 Hi team,
Can you help to review below schematic.
For the CDCLVC1310, can we connect all the GND pin together as below:
Lacey
Thanks a lot!
Part Number: CDCLVC1310 Other Parts Discussed in Thread: LMK00101 Dear team,
When using a CDCLVC1310 as a clock buffer, the input voltage level is 3.3V. If we want to get 1.8V and 3.3V voltage output signal at the same time on one chip.
Does this…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: LMK00101 , LMK00105 Hi Team,
How are the four pins VDDO map to the output channel 0~9 ? If one of the VDDo pin no power, which output channel will be influenced?
Thank you.
Part Number: CDCLVC1310 Hi team,
My customer are using the CDCLVC1310. The input is the 100M crystal oscillator and output 10 different frequency clock.
But the 500M,900M and 1.6GHz output signal has high level RF radiation, can't pass the RF radiation…
Part Number: LMK00301 Other Parts Discussed in Thread: CDCLVC1310 Hi team,
When my customer use the LMK00301 and CDCLVC1310, there is a situation that they power off the units but remain input the clock signal in the input pin.
So my customer want…