Part Number: CDCLVC1310 Hi team,
When customer is estimating CDCLVC1310 device, they found the minimum value of VOH is 0.7*VDDO when VDDO voltage is below 2V. And the spec of other manufactures' chip is 0.8*VDDO. As customer has the requirement for…
Part Number: CDCLVC1310-EVM Hi I'm building a clock distribution network using a 10Mhz Rubidium standard as an input signal. The signal is a sine wave (1.5Vpp). The other instruments (that should be provided with this clock reference) require a square…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: CDC3RL02 Hi team,
My customer is looking for a 52Mhz 1.8v Clipped-sine(sine clock from 0v to 1.8v peak to peak), the output is about 0.8v or 1.2v. LVCOMS output Do you have a clock
buffer like…
Part Number: CDCLVC1310 Hi team,
My customer is using CDCLVC1310, and they have a requirement on the output available time after power up.
They hope that all outputs could be stable within 10ms after power up.
Can we guarantee it?
Thanks
Part Number: CDCLVC1310 Hi team,
I have a question about the bypass mode for the crystal-oscillator input.
If I set the input clock select pin to 11, it means I choose the XTAL bypass mode.
So it means I can connect a 50MHz crystal-oscillator directly…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: CDCLVC1104 , CDCLVC1103 , LMK00804B , LMK00105 Is there a 3-4 output flavour of CDCLVC1310 also available?
Part Number: CDCLVC1310 Hi Team,
Do we need a termination network to bias the input signal to VDD/2 for AC couple LVCOMS input signal? There is already internal bias circuit in PRI/SEC input to VDD/2,but there is the termination network at the input…
Part Number: CDCLVC1310 I intend to stage two CDCLVC1310, i.e. on part will be driven by the LVCMOS output of the other. I was wandering if I can use only series termination only?
The section for INPUT CHARACTERISTICS is ambiguous in the datasheet as…
Part Number: CDCLVC1310 Hi team,
My customer wants to use CDCLVC1310's XIN input as SE LVCMOS input. And VDD is 3.3V.
What'll be the VIH & VIL of XIN input in such configuration?
Thank you.
Part Number: CDCLVC1310 Trying to understand Crystal recommendation. Not directly related to cdclvc1310 though.
What happens if I select a Crystal with a different load capacitance than recommended in Datasheet.
Instead of 25MHz, 16pf, if I select…